Part Number: TM4C1294KCPDT
Other Parts Discussed in Thread: ENERGIA
Hi,
Is it possible to define the period of PWM during initialization.?
Or define the status of PWM pins during initialization.
Regards
Nikhil
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: TM4C1294KCPDT
Other Parts Discussed in Thread: ENERGIA
Hi,
Is it possible to define the period of PWM during initialization.?
Or define the status of PWM pins during initialization.
Regards
Nikhil
Nikhil KV1 said:Is it possible to define the period of PWM during initialization.?
Or define the status of PWM pins during initialization.
Yes - to both questions. (assumes that 'initialization' is 'sharpened' to 'PWM Module Initialization.'
(*) only a select number of MCU's GPIOs may perform with 'official' PWM capability. The MCU's manual fully describes/details.
Hi,
Without calling PWM_open(), and only PWM_init() function is called.
That is before calling PWM_open() function is it possible to execute PWMGenPeriodSet and PWMPulseWidthSet APIs.?.
During PWM_init() time itself is it possible to set the PWM period and and Duty cycle.?.
Regards
Nikhil
Nikhil KV1 said:Without calling PWM_open(), and only PWM_init() function is called.
Are those 2 functions resident w/in vendor's standard API? If 'energia' - directing such question 'to that source' proves best.
Kindly note - NO mention of (the assumed) 'energia' appeared earlier - nor does it arrive (even) now.
You may 'tease out' such answers via careful & controlled experimentation. Be sure to disconnect any/all Motors or other 'loads' - which 'had' earlier attached to your PWM and/or connected Power Stage.
A current-limited LED proves an effective 'PWM Monitor.' You may then, 'Step thru your code' - while observing the Led - thus enabling you to, 'Note the impact of individual function calls' - in a 'SAFE & CONTROLLED Manner!'
Hi Nikhil,
You are asking a TI-RTOS question that you didn't clarify in the beginning of your post. The PWM_Params_init() initializes an PWM_Params data structure while the PWM_open() initializes a given PWM instance (i.e. PWM0, PWM1 or etc). So to answer your question, without calling the PWM_open() on the specified PWM instance, you cannot have the effect of the period/duty on that instance.