Part Number: EK-TM4C1294XL
Other Parts Discussed in Thread: ENERGIA
Tool/software: TI C/C++ Compiler
Good Morning,
(I'm brazilian, so some language problems can happen in my text, sorry)
Recently I bought the EK-TM4C1294XL board and in the first time that I had tried to load data to my board the problem in attachment happened. I already had tried to change the port usb in my computer in the software, but the same problem still was happing.. This considering I had Tried to load the exemple "blink".
Energia: 1.8.7E21 (Windows 10), Placa:"LaunchPad (Tiva C) w/ tm4c129 (120MHz)"
O sketch usa 3944 bytes (0%) de espaço de armazenamento para programas. O máximo são 1048576 bytes.
Variáveis globais usam 616 bytes (0%) de memória dinâmica, deixando 261528 bytes para variáveis locais. O máximo são 262144 bytes.
DSLite version 7.2.0.2096
Configuring Debugger (may take a few minutes on first launch)...
Initializing Register Database...
Parsing C:\Users\USURIO~2\AppData\Local\TEXASI~1\CCS\tools\0\0\2908048564.cache
Parsing C:\Users\Usuário1\AppData\Local\Energia15\packages\energia\tools\dslite\7.2.0.2096\common\targetdb\Modules\cs_dap_NotVisible.xml
Failed: Cannot read System Setup data from XML file C:\Users\Usuário1\AppData\Local\Energia15\packages\energia\tools\dslite\7.2.0.2096/EK-TM4C1294XL.ccxml
Could not open file "C:\Users\Usuário1\AppData\Local\Energia15\packages\energia\tools\dslite\7.2.0.2096\common\targetdb\Modules\cs_dap_NotVisible.xml"
Ocorreu um erro enquanto o sketch era carregado