Because of the Thanksgiving holiday in the U.S., TI E2E™ design support forum responses may be delayed the week of November 23.

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TM4C1290NCPDT: ISR on PQ2

Part Number: TM4C1290NCPDT

startup_ccs.c file

 IntDefaultHandler,                      // GPIO Port Q (Summary or Q0)

 ResetDebugISR,                      // GPIO Port Q2

I need to check if interrupt on PQ2 has triggered.. Is the API for interrupt status correct?

I don't have any other interrupt on port Q except on pin PQ2.

Thanks,

Priya

void ResetDebugGPIO_Initialize(void)
{
    ROM_SysCtlPeripheralEnable(SYSCTL_PERIPH_GPIOQ);
    resetDbgIntTriggered = 0;
      //Set Pin as input
    GPIOPinTypeGPIOInput(GPIO_PORTQ_BASE, GPIO_PIN_2);
    GPIOIntRegisterPin(GPIO_PORTQ_BASE, GPIO_PIN_2, ResetDebugISR); //Temp Disable 09-20-2017
    GPIOIntTypeSet(GPIO_PORTQ_BASE, GPIO_PIN_2, GPIO_RISING_EDGE);
    GPIOIntEnable(GPIO_PORTQ_BASE, GPIO_PIN_2);
}
void ResetDebugISR(void)
{
    bool bMasked = false;
    uint32_t intStatus = 0;
        //Check if this is a GPIO Interrupt
        intStatus = GPIOIntStatus(GPIO_PORTQ_BASE, bMasked);
        if((intStatus & GPIO_PIN_2) == GPIO_PIN_2)
        {
            //CLEAR THE INTERUPT
            resetDbgIntTriggered = 1;
            GPIOIntClear(GPIO_PORTQ_BASE, GPIO_PIN_2);
            GPIOIntDisable(GPIO_PORTQ_BASE, GPIO_PIN_2);
            resetDbgIntTriggered = 0;
        }
}
//PN
edited to remove ROM defines
  • Hi,

      I don't see a problem with your code with a quick glance. Do you see the interrupt tripped if you place a breakpoint on the ResetDebugISR?

      I assume somewhere in your code, not shown here will enable interrupt at the NVIC level and also enable the processor interrupt. 

      

  • No. That's the reason why I am having my code reviewed. I have requested a jumper at pin PQ2 to confirm on the scope when I trigger the ISR.

    Thanks,

    Priya

  •   I assume somewhere in your code, not shown here will enable interrupt at the NVIC level and also enable the processor interrupt. 

    Can you show an example of this?

    IntMasterEnable is called before the while(){} loop begins

    IntPrioritySet(INT_GPIOQ2, (PRIORITY_LEVEL_1 ));     //PN

    GPIOIntRegisterPin API registers the PQ2 ISR.

    edited to add all init APIs

  • Here is one example I have on the PJ0 pin looking for a falling edge to generate interrupt.

        SysCtlPeripheralEnable(SYSCTL_PERIPH_GPIOJ);
        while(!(SysCtlPeripheralReady(SYSCTL_PERIPH_GPIOJ)));
        GPIOPinTypeGPIOInput(GPIO_PORTJ_BASE, GPIO_PIN_0);
        GPIOPadConfigSet(GPIO_PORTJ_BASE, GPIO_PIN_0, GPIO_STRENGTH_2MA, GPIO_PIN_TYPE_STD_WPU);
        GPIOIntTypeSet(GPIO_PORTJ_BASE, GPIO_PIN_0, GPIO_FALLING_EDGE);
        GPIOIntRegister(GPIO_PORTJ_BASE, SW1Handler);
        GPIOIntEnable(GPIO_PORTJ_BASE, GPIO_INT_PIN_0);
        IntEnable(INT_GPIOJ);
        //
        // Enable processor interrupts.
        //
        IntMasterEnable();

  • Greetings,

    Note:  Swear to God - Charles' post (above) was not present when I joined the thread.     Even so - it is believed that 'code alone' may not (fully) satisfy this poster.

    Priya Nadathur70 said:
    GPIOIntTypeSet(GPIO_PORTQ_BASE, GPIO_PIN_2, GPIO_RISING_EDGE);

    Should not pin 'PQ2' be equipped with:

    • either the MCU's (weak) pull-down (resistor) or an external one   (Charles' post included a 'pull-up')
    • and some method to, 'Generate a logic-high' - felt at PQ2     (this requirement was (yet) to be described)
    • it appears that 'PQ2' is presently 'floating' - which is 'never' good - and (even) worse when employed as a, 'Pin Interrupt.'    (Charles 'pull-up' resolved)

    It should be noted that if poster's application (demands) the detection of a 'Rising Edge' - the 'weak pull-up' w/in the verified code must be replaced w/'Weak pull-down')

    If a scope is not available you may program your ISR to 'toggle' another pin on Port_'Q' - and have that pin drive a (current-limited) Led.   (that will confirm that your ISR (was) entered.)

    Note that if a 'simple switch' is used to 'trigger the PQ2 interrupt' - that switch will (surely) 'bounce' - and the interrupt may be entered (several) times.    You may 'resolve that 'bounce' by employing (another) Port_Q pin  (set as output) to 'single pulse' PQ2...