Part Number: TM4C1290NCPDT
In one of our new designs using TM4C1294 controller.
We need 2CAN and 1 USB. Shall we make connections as shown in figure (attached)
Since Pin 95 and 96 are being used for CAN, we could not connect USB_VBUS and USB_ID to TM4C1294 controller.
My questions are:
1) Since PB0/Pin 95 and PB1/Pin96 are multipexed with both USB and CAN. Is this configuration valid?
2) If answer for above is "yes" then
a) How to connect USB_VBUS at the USB connector?
b) How to connect USB_ID at the USB connector?
Thanks in Advance
HARANATH V