Part Number: EM1402EVM
Other Parts Discussed in Thread: BQ76PL455A-Q1
Hi,
I'm using EM1402EVM together with LAUNCHXL-TMS57004. I have some questions about the BMS and the Battery Module.
1) In the TI Design it says that the active cell balancing works with and an external 12-V supply or with another battery pack. Does this means that the active cell balancing doesn't work or the EV1402 doesn't work? Can I still monitoring the battery module with the BQ76PL455A-Q1?
2) Can I monitor the charge and discharge while the battery pack supply a Driver motor + BLDC motor?
3) Can I connect the external 12V supply connectors to the battery module to charge or discharge one cell of the battery with the battery module itself? (it may be confusing)
Thanks.