Because of the Thanksgiving holiday in the U.S., TI E2E™ design support forum responses may be delayed the week of November 23.

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS570LC4357: Number of ADC inputs

Part Number: TMS570LC4357
Other Parts Discussed in Thread: TMS570LS3137

Hello,

The dev board that I'm using, TMS570LC43HDK, only has 24 ADC1 and 16 ADC2 inputs. There is also a mention of this (24/16) in the TRM, specifically in Table 22-1. ADC Look-Up Table Field Descriptions.

However, the data sheet specifies 32/25 everywhere (including the BGA map) and other places in the TRM also specify the same.

So, I assume the device has 32/25 capable ADC1/2 inputs, however I just wanted to verify and also understand why this dev board does not have all the inputs. Is there another dev board that does support all ADC inputs?

Thanks,
Kevin