Part Number: TM4C1290NCPDT
Tool/software: Code Composer Studio
Hi,
My customer is reported an error with CCS when the target is connected.
Please see attached console snap shot.
It says “CS_DAP_0: GEL: Error while executing GEL_Reset(): A reset is not allowed at this time at GEL_Reset()”,
but no GEL_Reset() is called in GEL file as attached.
What cause the error?
/* tm4c1290ncpdt.gel
*
* Revisions:
* June-10-2014 3rd revision
*
* This is derived from revision 15071 of the TivaWare Library.
*
*/
menuitem "StartUp"
hotmenu StartUp()
{
/* Load the CortexM3_util.gel file */
GEL_LoadGel("$(GEL_file_dir)/CortexM3_util.gel");
GEL_MapOff();
GEL_MapReset();
GEL_MapOn();
memorymap_init();
}
OnTargetConnect()
{
}
memorymap_init()
{
/*
* Syntax for GEL_MapAddStr.
* GEL_MapAddStr(address, page, length, "attribute", waitstate);
Basic Attribute Types Derived Attribute Types
String Description String Description
R Read NONE No memory/protected
W Write RAM Read and write
P Port ROM Read only
EX External WOM Write only
EM Emulator INPORT Port read only
PR Programmable OUTPORT Port write only
ER Erasable IOPORT Port read and write
DA Dual access SARAM Single access RAM
ASn Access size DARAM Dual access RAM
SHnC Shared FLASH Flash ROM
CACHE Cache EXRAM External RAM
TX Text EXROM External ROM
MN Monitor EPROM Erasable write-able EPROM
SA Single access MONITOR Monitor ROM
FL Flash PRAM Program RAM
MR Memory mapped PROM Program ROM
NULL NULL NULL NULL
*/
GEL_MapAddStr(0x00000000, 0, 0x00100000, "R", 0); /* Flash */
GEL_MapAddStr(0x01000000, 0, 0x00008c00, "R", 0); /* ROM */
GEL_MapAddStr(0x20000000, 0, 0x00040000, "R|W", 0); /* SRAM */
GEL_MapAddStr(0x40000000, 0, 0x00001000, "R|W", 0); /* WATCHDOG0 */
GEL_MapAddStr(0x40001000, 0, 0x00001000, "R|W", 0); /* WATCHDOG1 */
GEL_MapAddStr(0x40008000, 0, 0x00001000, "R|W", 0); /* SSI0 */
GEL_MapAddStr(0x40009000, 0, 0x00001000, "R|W", 0); /* SSI1 */
GEL_MapAddStr(0x4000A000, 0, 0x00001000, "R|W", 0); /* SSI2 */
GEL_MapAddStr(0x4000B000, 0, 0x00001000, "R|W", 0); /* SSI3 */
GEL_MapAddStr(0x4000C000, 0, 0x00001000, "R|W", 0); /* UART0 */
GEL_MapAddStr(0x4000D000, 0, 0x00001000, "R|W", 0); /* UART1 */
GEL_MapAddStr(0x4000E000, 0, 0x00001000, "R|W", 0); /* UART2 */
GEL_MapAddStr(0x4000F000, 0, 0x00001000, "R|W", 0); /* UART3 */
GEL_MapAddStr(0x40010000, 0, 0x00001000, "R|W", 0); /* UART4 */
GEL_MapAddStr(0x40011000, 0, 0x00001000, "R|W", 0); /* UART5 */
GEL_MapAddStr(0x40012000, 0, 0x00001000, "R|W", 0); /* UART6 */
GEL_MapAddStr(0x40013000, 0, 0x00001000, "R|W", 0); /* UART7 */
GEL_MapAddStr(0x40020000, 0, 0x00001000, "R|W", 0); /* I2C0 */
GEL_MapAddStr(0x40021000, 0, 0x00001000, "R|W", 0); /* I2C1 */
GEL_MapAddStr(0x40022000, 0, 0x00001000, "R|W", 0); /* I2C2 */
GEL_MapAddStr(0x40023000, 0, 0x00001000, "R|W", 0); /* I2C3 */
GEL_MapAddStr(0x40028000, 0, 0x00001000, "R|W", 0); /* PWM0 */
GEL_MapAddStr(0x4002C000, 0, 0x00001000, "R|W", 0); /* QEI0 */
GEL_MapAddStr(0x40030000, 0, 0x00001000, "R|W", 0); /* TIMER0 */
GEL_MapAddStr(0x40031000, 0, 0x00001000, "R|W", 0); /* TIMER1 */
GEL_MapAddStr(0x40032000, 0, 0x00001000, "R|W", 0); /* TIMER2 */
GEL_MapAddStr(0x40033000, 0, 0x00001000, "R|W", 0); /* TIMER3 */
GEL_MapAddStr(0x40034000, 0, 0x00001000, "R|W", 0); /* TIMER4 */
GEL_MapAddStr(0x40035000, 0, 0x00001000, "R|W", 0); /* TIMER5 */
GEL_MapAddStr(0x40038000, 0, 0x00001000, "R|W", 0); /* ADC0 */
GEL_MapAddStr(0x40039000, 0, 0x00001000, "R|W", 0); /* ADC1 */
GEL_MapAddStr(0x4003C000, 0, 0x00001000, "R|W", 0); /* COMP */
GEL_MapAddStr(0x40040000, 0, 0x00001000, "R|W", 0); /* CAN0 */
GEL_MapAddStr(0x40041000, 0, 0x00001000, "R|W", 0); /* CAN1 */
GEL_MapAddStr(0x40050000, 0, 0x00001000, "R|W", 0); /* USB0 */
GEL_MapAddStr(0x40058000, 0, 0x00001000, "R|W", 0); /* GPIO PORTA AHB */
GEL_MapAddStr(0x40059000, 0, 0x00001000, "R|W", 0); /* GPIO PORTB AHB */
GEL_MapAddStr(0x4005A000, 0, 0x00001000, "R|W", 0); /* GPIO PORTC AHB */
GEL_MapAddStr(0x4005B000, 0, 0x00001000, "R|W", 0); /* GPIO PORTD AHB */
GEL_MapAddStr(0x4005C000, 0, 0x00001000, "R|W", 0); /* GPIO PORTE AHB */
GEL_MapAddStr(0x4005D000, 0, 0x00001000, "R|W", 0); /* GPIO PORTF AHB */
GEL_MapAddStr(0x4005E000, 0, 0x00001000, "R|W", 0); /* GPIO PORTG AHB */
GEL_MapAddStr(0x4005F000, 0, 0x00001000, "R|W", 0); /* GPIO PORTH AHB */
GEL_MapAddStr(0x40060000, 0, 0x00001000, "R|W", 0); /* GPIO PORTJ AHB */
GEL_MapAddStr(0x40061000, 0, 0x00001000, "R|W", 0); /* GPIO PORTK */
GEL_MapAddStr(0x40062000, 0, 0x00001000, "R|W", 0); /* GPIO PORTL */
GEL_MapAddStr(0x40063000, 0, 0x00001000, "R|W", 0); /* GPIO PORTM */
GEL_MapAddStr(0x40064000, 0, 0x00001000, "R|W", 0); /* GPIO PORTN */
GEL_MapAddStr(0x40065000, 0, 0x00001000, "R|W", 0); /* GPIO PORTP */
GEL_MapAddStr(0x40066000, 0, 0x00001000, "R|W", 0); /* GPIO PORTQ */
GEL_MapAddStr(0x400AF000, 0, 0x00001000, "R|W", 0); /* EEPROM */
GEL_MapAddStr(0x400B8000, 0, 0x00001000, "R|W", 0); /* I2C8 */
GEL_MapAddStr(0x400B9000, 0, 0x00001000, "R|W", 0); /* I2C9 */
GEL_MapAddStr(0x400C0000, 0, 0x00001000, "R|W", 0); /* I2C4 */
GEL_MapAddStr(0x400C1000, 0, 0x00001000, "R|W", 0); /* I2C5 */
GEL_MapAddStr(0x400C2000, 0, 0x00001000, "R|W", 0); /* I2C6 */
GEL_MapAddStr(0x400C3000, 0, 0x00001000, "R|W", 0); /* I2C7 */
GEL_MapAddStr(0x400D0000, 0, 0x00001000, "R|W", 0); /* EPI0 */
GEL_MapAddStr(0x400E0000, 0, 0x00001000, "R|W", 0); /* TIMER6 */
GEL_MapAddStr(0x400E1000, 0, 0x00001000, "R|W", 0); /* TIMER7 */
GEL_MapAddStr(0x400F9000, 0, 0x00001000, "R|W", 0); /* SYSEXC */
GEL_MapAddStr(0x400FC000, 0, 0x00001000, "R|W", 0); /* HIB */
GEL_MapAddStr(0x400FD000, 0, 0x00001000, "R|W", 0); /* FLASH CTRL */
GEL_MapAddStr(0x400FE000, 0, 0x00001000, "R|W", 0); /* SYSCTL */
GEL_MapAddStr(0x400FF000, 0, 0x00001000, "R|W", 0); /* UDMA */
GEL_MapAddStr(0x44030000, 0, 0x00001000, "R|W", 0); /* CCM0 */
GEL_MapAddStr(0xE000E000, 0, 0x00001000, "R|W", 0); /* NVIC */
GEL_TextOut("\nMemory Map Initialization Complete\n");
}
Thanks and regards,
Koichiro Tashiro