Part Number: TMS570LS3137
Other Parts Discussed in Thread: HALCOGEN
Tool/software: Code Composer Studio
CCS 8.2.0.00007
Is it possible to exclude from a build those procedures that are not called?
HALCoGen (4.7.0) produces utility procedures for the peripherals. Many of these I do not use. How can I exclude them from the build?
I cannot find an appropriate option in the CCS ARM Linker section.
Do I have to remove them manually?
Regards,
Tom Pikett