Part Number: TMS570LC4357
Hi Team,
Here is a question from customer.
customer found ERROR pin is pulled down and find ESM Group2 bit3 is set. Based on datasheet, it seems it's related with flash ECC.
Then check FLASH related Regs: FEDAC_PASTATUS, FEDAC_PBSTATUS, FEDAC_GBLSTATUS are both 0.
Also, have suggested customer to check EPC description, and they found CAM_CONTENT[0], CAM_CONTENT[1], CAM_CONTENT[3] changes. CAM_CONTENT[0]=0x000802F8, CAM_CONTENT[1]=0x00080300, CAM_CONTENT[3]=0x0080318.
Based on datasheet, it only shows" CPU writes to this field in function or diagnostic mode. the write data is maksed with byten and stored into CAM on each index" . But no description on meanings of those Regs. Does it mean the address that fault happens? what can be done next to analysis the reason based on the value in Regs? Thanks.
BRs
Given