Hello,
An example code for RTI DWWD usage works perfectly. I was wondering what happens if I try to write the WDKEY key values without enabling the counter? Tried doing that and my system goes into a complete hang state:
"Trouble Halting Target CPU:
(Error -1060 @ 0x0)
Device is not responding to the request.
Reset the device, and retry the operation.
If error persists, confirm configuration, power-cycle the board, and/or try more reliable JTAG settings *e.g. lower TCLK).
(Emulation package 5.0.747.0)"
I am confident that the issue is with accessing the WDKEY before enabling the counter and couldn't find any information relating to it in the ref manuals. Any information on the system state when this happens would be helpful.
Thank you!