Part Number: TMS570LS1224
Other Parts Discussed in Thread: UNIFLASH
Tool/software: Code Composer Studio
Dear Support Team,
I'm currently using the RTBox by Plexim and a Hercules TMS570LS1224 Launchpad to do HIL testing.
Plexim offers an Adapterboard which allows a very simple connection between the Launchpads and the RTBox.
On this adapterboard, a 3.3. Voltage is used to supply the Launchpad with the first Pin on the J1 Header.
My question now is: Is it possible, to communicate with the XDS110 Debug probe from the launchpad and flash software via the USB Port while also having this external power supply?
I have tried several jumper configurations only to receive one of the following errors:
Trying to flash with CCS 9.3:
Error connecting to the target:
(Error -2062 @ 0x0)
Unable to halt device. Reset the device, and retry the operation. If error persists, confirm configuration, power-cycle the board, and/or try more reliable JTAG settings (e.g. lower TCLK).
(Emulation package 8.3.0.00003)
Trying to erase Flash with Uniflash:
Error connecting to the target:
(Error -241 @ 0x0)
A router subpath could not be accessed. A security error has probably occurred. Make sure your device is unlocked.
(Emulation package 8.2.0.00004)
The emulation package should be 8.3 though.
Thank for your help,
Sebastian