Part Number: RM48L952
How we need to map the address/memory for 8-bit/16-bit Flash/SRAM using EMIF I/F of RM48L952 Microcontroller ? and what is the reason behind these type of mapping ?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: RM48L952
How we need to map the address/memory for 8-bit/16-bit Flash/SRAM using EMIF I/F of RM48L952 Microcontroller ? and what is the reason behind these type of mapping ?
Hello,
Section 17.2.6.1 in device TRM describes interfacing to 8/16 bit Asynchronous Memory.
Of special note is the connection between the EMIF and the external device's address bus. The EMIF address pin EMIF_A[0] always provides the least significant bit of a 32-bit word address. Therefore, when interfacing to a 16-bit or 8-bit asynchronous device, the EMIF_BA[1] and EMIF_BA[0] pins provide the least-significant bits of the halfword or byte address, respectively. Additionally, when the EMIF interfaces to a 16-bit asynchronous device, the EMIF_BA[0] pin can serve as the upper address line EMIF_A[22].
Hello,
It is by design. I am not aware with the silicon design decisions.
By design The EMIF address pin EMIF_A[0] always provides the least significant bit of a 32-bit word address. Therefore additional signals for 8bit and 16bit addressing are required.