Because of the Thanksgiving holiday in the U.S., TI E2E™ design support forum responses may be delayed the week of November 23.

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CCS/TM4C1294NCPDT: Problem enabling DHCP together with BOOTP

Part Number: TM4C1294NCPDT

Tool/software: Code Composer Studio

Hi

I have a slightly complex problem ...

My project is capable of switching between static IP and dynamic IP perfectly.

lwIPNetworkConfigChange(0, 0, 0, IPADDR_USE_DHCP);

or

lwIPNetworkConfigChange(DEF_Ip, DEF_Mask, DEF_Gateway,IPADDR_USE_STATIC);

Then I implemented in my code a routine for firmware update through the ethernet port.

while(1)
{

//...


    if(g_bFirmwareUpdate == 0x72)
    {
        ROM_GPIOPinWrite(GPIO_PORTN_BASE, GPIO_PIN_1, GPIO_PIN_1);
        SoftwareUpdateBegin(g_ui32SysClock);
    }

}

However, after that, I noticed that every time I try to change from static to dynamic IP, my code goes into FaultISR.

Debugging the code, I noticed that it fails to access the function "mem_malloc()", located in "mem.c" just before line 77.

The big question would be: Why did it work well before enabling ethernet firmware upgrade? And what changed to make the code crash after that?

Remember that if I have static IP, the firmware update works correctly ...

I am not getting a solution to this problem, but I believe it may have something related to port 68 used by DHCP and BOOTP.

Looking at the example "boot_emac_flash" it is possible to change the ports used during the upgrade in the file "bl_emac.c"

//*****************************************************************************
//
// The UDP ports used by the BOOTP protocol.
//
//*****************************************************************************
#define BOOTP_SERVER_PORT       67
#define BOOTP_CLIENT_PORT       68

//*****************************************************************************
//
// The UDP port for the TFTP server.
//
//*****************************************************************************
#define TFTP_PORT               69

I'm really not sure if this is really the problem... But is there any way to change these ports without using the "boot_emac_flash" initializer in my project?

Or if my suspicions are wrong, can anyone see what other cause this problem could have?

Thanks!