Part Number: TMS570LS3137
Tool/software: Code Composer Studio
Hello,
I have been trying to program/debug a TMS570LS3137 mounted on my own PCB for several hours. I use an XDS110 Debug Probe. However, after several attempts, it is impossible to program and debug. I always get the same error which is the following:
"Error connecting to the target:
(Error -1170 @ 0x0)
Unable to access the DAP. Reset the device, and retry the operation. If error persists, confirm configuration, power-cycle the board, and/or try more reliable JTAG settings (e.g. lower TCLK).
(Emulation package 8.2.0.00004)"
Here are the different things I tried to do that didn't work:
- Check the hardware connections
- Decrease the frequency in target configuration (100kHz)
- Use a "Test Connection" that gives me a success
- Read the different points in this post which didn't help me: http://e2e.ti.com/support/microcontrollers/hercules/f/312/t/785145?CCS-TMS570LC4357-Error-1170-Unable-to-access-the-DAP
By following this post (https://e2e.ti.com/support/microcontrollers/hercules/f/312/p/542615/2020352I managed to erase all the flash. However, then, when I want to load my program, just at the end of the loading, I get the same errors as usual:
I would like to point out that my PCB is a version 2 of another almost similar PCB, where I can flash and program without any problem. In these new PCBs, I never managed to program.
Thank you in advance for your help:) !
Maxime