Part Number: TMS570LC4357
Hi,
I want to generate two events with eTPWM configuration. (1) On start of each PWM cycle. (2) at 50% of TBPRD value. For (1) I am using eTPWM Interrupt event, and for (2) want to use SOCB. I am able to generate the events as required only at 50% duty cycle. For all other value of duty cycle change, the SOCB trigger is changing the timing. Do we have a solution which can create reliable events.
Best Regards,
Chandra