Part Number: TM4C1294KCPDT
Hi all,
I know TivaWare supports device CDC driver, does it support host CDC driver as well?
Luke
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: TM4C1294KCPDT
Hi all,
I know TivaWare supports device CDC driver, does it support host CDC driver as well?
Luke
Hello Luke,
The current release does not, but I have developed the host CDC driver for the next release. I can share the library files and example here. I don't believe any additional files are needed beyond these new ones I am sharing.
Files to add to usblib/host folder: usblib_host_cdc_files.zip
Example project: 7144.usb_host_serial.zip
Hello Ralph,
This is EXCELLENT NEWS - thank you!
May these files be freely used by 'other forum users' - as well as T.I.'ers?
Have these 'had time' to receive 'normal/customary' T.I. sanctioned 'Test & Evaluation?'
Again thanks...
Hello cb1,
I have tested the example and verified the functionality with USB analyzer, but from an application standpoint I may make an improvement before final release to setup a more compelling demonstration between device and host projects. And the files include standard TI licensing terms in the headers.