Part Number: TM4C1294NCPDT
Hello,
After the last few days of diving into the EPI interface and how to get it functioning with a Zilog Z16C30 Universal Serial Controller i have come to an issue with writing and reading. I have double checked with the manufacturer of the Zilog part on what their correct initialization routine should be based on a previous development kit they produced. However i noticed that the data being sent from the serial controller did not look correct. Thinking that loopback mode might help alleviate some of the concerns i implemented that, although when i read the register that should hold the data that was send i only see the register index returned and no data. Attached is the current configuration of the EPI Driver along with the configuration of the universal serial controller and read/write of data for the serial bus.
Any help would be appreciated,
David
/*
* EPI.c
*
* Created on: Nov 1, 2019
* Author: harrida
*/
#include <stdint.h>
#include <stdbool.h>
#include <string.h>
#include "inc/hw_ints.h"
#include "inc/hw_memmap.h"
#include "inc/hw_types.h"
#include "inc/hw_epi.h"
#include "inc/hw_gpio.h"
#include "driverlib/debug.h"
#include "driverlib/fpu.h"
#include "driverlib/gpio.h"
#include "driverlib/interrupt.h"
#include "driverlib/pin_map.h"
#include "driverlib/rom.h"
#include "driverlib/rom_map.h"
#include "driverlib/sysctl.h"
#include "driverlib/timer.h"
#include "driverlib/epi.h"
#include "driverlib/udma.h"
#include "Inc/MicrocontrollerDefinitions.h"
#include "Drivers/EPI.h"
static volatile uint16_t *g_pui16EPISdram;
void InitalizeEPIDriver(void)
{
// RESET pm6
GPIOPinWrite(GPIO_PORTM_BASE, GPIO_PIN_6, 0);
SysCtlDelay(10000);
GPIOPinWrite(GPIO_PORTM_BASE, GPIO_PIN_6, GPIO_PIN_6);
SysCtlDelay(10000);
EPIModeSet(EPI0_BASE, EPI_MODE_HB16); //general mode EPI_MODE_GENERAL EPI_MODE_HB16
EPIDividerSet(EPI0_BASE, 0x0A0A); //1=60MHz, 10=10MHz, 119=1MHz Sets the clock divider for the EPI module�s CS0n/CS1n.
EPIConfigHB16Set(EPI0_BASE,
EPI_HB16_MODE_ADMUX | //sets data and address muxed, AD[15:0].
EPI_HB16_WRWAIT_3 | //sets write wait state to 2 EPI clocks.
EPI_HB16_RDWAIT_3 | //sets read wait state to 2 EPI clocks.
EPI_HB16_CLOCK_GATE_IDLE| // holds the EPI clock low when no data is available to read or write.
EPI_HB16_ALE_LOW| //sets address latch active low.
EPI_HB16_CSCFG_ALE_DUAL_CS,// sets EPIS030 as an address latch (ALE),
//! EPIS027 as CS0n and EPIS026 as CS1n with the asserted chip select
//! determined from the most significant address bit for the respective
//! external address map.
1); // the maximum number of external clocks to wait if a FIFO ready signal is
//holding off the transaction.
EPIAddressMapSet(EPI0_BASE,
EPI_ADDR_PER_SIZE_256MB | //256MB location
EPI_ADDR_PER_BASE_A); //EPI0 is mapped from 0xA0000000 to 0xA00000FF.
// READ WRITE OPERARION FOR VERIFICATION
// Write BCR:
// SepAd = 0 as this is 16 bits wide
// 16-Bit = 1 for 16-bit operation
// 2PulseAck = 0 as PITACK is not used
// SRightA = 1
g_pui16EPISdram = (uint16_t *)0xA0000000;
g_pui16EPISdram[0x05] = 0x0005;
SetRegisterConfiguration(0x80);
SetRegisterConfiguration(0x00);
}
void GetEPIData(uint16_t value)
{
uint16_t testA = 0;
uint16_t testB = 0;
// Set the EPI memory pointer to the base of EPI memory space. Note that
// g_pui16EPISdram is declared as volatile so the compiler should not
// optimize reads out of the memory. With this pointer, the memory space
// is accessed like a sim*ple array.
g_pui16EPISdram = (uint16_t *)0xA0000000;
// READ WRITE OPERARION FOR VERIFICATION
//g_pui16EPISdram[0 + 0x1C] = 0xFFFF; // MISR
//g_pui16EPISdram[58] = 2;//value;
g_pui16EPISdram[48] = 1;//value;
testB = g_pui16EPISdram[32];
//g_pui16EPISdram[186] = 2;//value;
g_pui16EPISdram[176] = 1;//value;
testA = g_pui16EPISdram[160];
}
void SetRegisterConfiguration(uint8_t RegBase)
{
if(RegBase != 0 | RegBase != 0x80)
{
RegBase = 0x80;
}
// Setup for Register
//Zilog Support
//
//---------------------------------------------
// 2. Initializing the USC to HDLC mode (default)
//---------------------------------------------
// BCR
//> 0x0005 (uses 16-bit data; single pulse ack; multiplexed bus)
// CCAR
g_pui16EPISdram[RegBase + 0x00] = 0x0400; //(channel reset bit = 1)
g_pui16EPISdram[RegBase + 0x00] = 0x0000; //(channel reset bit = 0)
g_pui16EPISdram[RegBase + 0x00] = 0xB800; //(select D7-0 first)
// CMR
g_pui16EPISdram[RegBase + 0x02] = 0x1606; //(Tx/Rx mode HDLC, Tx Under Condition ABORT, No Preamble, Rx AddSearchmode disabled)
// RMR
g_pui16EPISdram[RegBase + 0x22] = 0x0600; //(Rx CRC Start = 1, RX CRC Enable = 1)
// TMR
g_pui16EPISdram[RegBase + 0x32] = 0x0700; //(Tx CRC Start = 1, Tx CRC Enable = 1 , Tx CRC at End = 1)
// CMCR
g_pui16EPISdram[RegBase + 0x10] = 0x0224; //(BRG1 clock source CTR0 output = 0x00, BRG0 clock source RxC pin = 0x10, DPLLSrc = 0x00, TxCLKSrc = 100, RxCLKSrc = 100
// IOCR
g_pui16EPISdram[RegBase + 0x16] = 0x0008; //(TxCMode = Drive /TxC with TxCLK)
// TC0R
g_pui16EPISdram[RegBase + 0x2E] = 0x009F; //(divisor value for 115200 baud for BRG0)
// TCSR
g_pui16EPISdram[RegBase + 0x34] = 0x6000;
// TICR
g_pui16EPISdram[RegBase + 0x36] = 0x0F00;
// TCSR
g_pui16EPISdram[RegBase + 0x34] = 0x7000;
// TICR
g_pui16EPISdram[RegBase + 0x36] = 0x0F00;
// TCSR
g_pui16EPISdram[RegBase + 0x34] = 0x0300;
// CCSR
g_pui16EPISdram[RegBase + 0x04] = 0x2000;
// CCR
g_pui16EPISdram[RegBase + 0x06] = 0x0080;
// RCLR
g_pui16EPISdram[RegBase + 0x2A] = 0xFFFF;
//---------------------------------------------
// 3. Enabling the USC
//---------------------------------------------
// HCR
g_pui16EPISdram[RegBase + 0x12] = 0x0001; // BRG0 Enable
// RMR
g_pui16EPISdram[RegBase + 0x22] = 0x0602; // Enable Rx , therefore 0x602
// TMR
g_pui16EPISdram[RegBase + 0x32] = 0x0702; // Enable Tx , therefore 0x702
// (Set Loopback part)
// CCAR
g_pui16EPISdram[RegBase + 0x00] = 0x0300; // (Mode Control, IntLocalLoopback)
// My Investigation
/* g_pui16EPISdram[RegBase + (0) << 1] = 0x0400; // CCAR
g_pui16EPISdram[RegBase + (0) << 1] = 0x0000; // CCAR
g_pui16EPISdram[RegBase + (0) << 1] = 0xB800; // CCAR
g_pui16EPISdram[RegBase + 0x16] = 0x0F36; // IOCR
//!
//! 0xc000
//! CTS Pin = 0x Active Low
//!
//! 0x3000
//! DCD Pin = 00 Active Low Rx Carrier
//!
//! 0x0c00
//! TxReq = 11 txReq Driven High
//!
//! 0x0e00
//! RxReq = 11 rxReg Driven High
//!
//! 0x00c0
//! TxD = 00 Transmitter Output
//!
//! 0x0038
//! TxC = 110 Output of CTR1
//!
//! 0x0007
//! RxC = 110 Output of CTR0
g_pui16EPISdram[RegBase + 0x10] = 0xF46C; // CMRC
//!
//! 0xc000
//! CTR1 Source = 11 CTR1 Source is TxC pin
//!
//! 0x3000
//! CTR0 SOurce = 11 CTR0 Source is TxC pin
//!
//! 0x0c00
//! BRG1 Source = 01 BRG1 Source is CTR1
//!
//! 0x0300
//! BRG0 Source = 00 BRG0 Source is CTR0
//!
//! 0x00c0
//! DPLL Source = 01 DPLL Source is BRG1
//!
//! 0x0038
//! TxCLKSrc = 101 BRG1 Ouput
//!
//! 0x0007
//! RxCLKSrc = 100 BRG0 Output
g_pui16EPISdram[RegBase + 0x2E] = 0x0001; // TC0R
g_pui16EPISdram[RegBase + 0x3E] = 0x0001; // TC1R
g_pui16EPISdram[RegBase + 0x12] = 0x50DD; // HCR
//!
//! 0xc000
//! CTR0 Divisor = 01 1/16
//!
//! 0x2000
//! CTR1 Divisor Select = 0 CTR0 Select
//!
//! 0x1000
//! CVOK = 1 Dont Report Violations
//!
//! 0x0c00
//! DPLL Divisor = 00 1/32
//!
//! 0x0300
//! DPLL Mode = 00 Disable
//!
//! 0x00c0
//! TxA Mode = 11 Drive High
//!
//! 0x0020
//! BRG1 Single Cycle = 0 Continuous
//!
//! 0x0010
//! BRG1 Enable = 1
//!
//! 0x000C
//! RxA Mode = 11 Drive High
//!
//! 0x0002
//! BRG0 Single Cycle = 0 Continuous
//!
//! 0x0001
//! BRG0 Enable = 1
g_pui16EPISdram[RegBase + 0x02] = 0x0626; // CMR
//!
//! 0xF000
//! TxSubMode
//!
//! 0x0F00
//! TxMode = 0110 HDLC Mode
//!
//! 0x00F0
//! RxSubMode = 0010 1 Byte Address, 1 Control Byte
//!
//! 0x000F
//! RxMode = 0110 HDLC Mode
//!
g_pui16EPISdram[RegBase + 0x04] = 0x2000; // CCSR
//!
//! 0x8000
//! RCC FIFO Overflow = 0
//!
//! 0x4000
//! RCC FIFO Not Empty = 0
//!
//! 0x2000
//! RCC Clear = 1
//!
//! 0x1000
//! DPLL In Sync
//!
//! 0x0800
//! DPLL Miss 2 Clocks
//!
//! 0x0400
//! DPLL Miss CLock
//!
//! 0x0300
//! DPLL Edge = 0
//!
//! 0x0080
//! HDLC In Loop
//!
//! 0x0040
//! HDLC Transmitting Loop
//!
//! 0x001F
//! Tx Residue = 000 Last HDLC Frame Contains 8 bits
//!
g_pui16EPISdram[RegBase + 0x06] = 0x1540; // CCR
//!
//! 0xC000
//! Tx Control BLocks = 00 no use
//!
//! 0x2000
//! Wait For Tx Trigger = 0
//!
//! 0x1000
//! Send Preamble flag = 1 send flag
//!
//! 0x0C00
//! Preamble = 01 16 bit Preamble
//!
//! 0x0300
//! Tx Preamble = 01 Preamble = all 1's
//!
//! 0x00C0
//! Rx Status Vlocks = 01 16 Bit
//!
//! 0x0020
//! Wait for Rx Trigger = 0
//!
g_pui16EPISdram[RegBase + 0x1C] = 0x8080; // DCCR
//!
//! 0xC000
//! Clear IUS Bits 10
//!
//! 0x00C0
//! Clear IP Bits 10
//!
g_pui16EPISdram[RegBase + 0x18] = 0x7E80; // ICR
//!
//! 0x8000
//! MIE enable Interrupts = 0
//!
//! 0x4000
//! Disable DLC Interrupt Enable Out = 1
//!
//! 0x2000
//! IntACK Cycle Vector = 1 Do not return
//!
//! 0x1E00
//! Interrupt Vectors = 1111 do not include status
//!
//! 0x00C0
//! INterrupt Operation = 10 - clear interrupts
g_pui16EPISdram[RegBase + 0x1C] = 0xAAA0; // MISR
//!
//! 0x8000
//! Rx CL/U = 1 Open Latches for RxC
//!
//! 0x4000
//! RxC value
//!
//! 0x2000
//! TxCL/U = 1 Open Latches for TxC
//!
//! 0x1000
//! TxC Value
//!
//! 0x0800
//! RxRl/U = 1 Open Latch for RxR
//!
//! 0x0400
//! RxR Value
//!
//! 0x0200
//! TxRL/U = 1 Open Latch for TxR
//!
//! 0x0100
//! TxR Value
//!
//! 0x0080
//! DCDL/U = 1 Open Latch for DcD
//!
//! 0x0040
//! DCD Value
//!
//! 0x0020
//! CTSL/U = 1 Open Latch for CTS
//!
//! 0x0010
//! CTS Value
g_pui16EPISdram[RegBase + 0x2A] = 0xFFFF; // RCLR
//!
//! Enable RCC no max frame/message
//!
g_pui16EPISdram[RegBase + 0x26] = 0x0000; // RICR
g_pui16EPISdram[RegBase + 0x34] = 0x0500; // TCSR
g_pui16EPISdram[RegBase + 0x3A] = 0x0000; // TCLR
g_pui16EPISdram[RegBase + 0x36] = 0x0000; // TICR
g_pui16EPISdram[RegBase + 0x22] = 0x0602; // RMR
g_pui16EPISdram[RegBase + 0x32] = 0x0602; // TMR
*/
/*g_pui16EPISdram[RegBase + 0] = 0x05;
g_pui16EPISdram[RegBase + (1) << 1] = 0x0606;
g_pui16EPISdram[RegBase + (2) << 1] = 0x05;
g_pui16EPISdram[RegBase + (3) << 1] = 0x05;
g_pui16EPISdram[RegBase + (4) << 1] = 0x05;
g_pui16EPISdram[RegBase + (5) << 1] = 0x05;
g_pui16EPISdram[RegBase + (6) << 1] = 0x05;
g_pui16EPISdram[RegBase + (7) << 1] = 0x05;
g_pui16EPISdram[RegBase + (8) << 1] = 0x05;
g_pui16EPISdram[RegBase + (9) << 1] = 0x05;
g_pui16EPISdram[RegBase + (10) << 1] = 0x05;
g_pui16EPISdram[RegBase + (11) << 1] = 0x05;
g_pui16EPISdram[RegBase + (12) << 1] = 0x05;
g_pui16EPISdram[RegBase + (13) << 1] = 0x05;
g_pui16EPISdram[RegBase + (14) << 1] = 0x05;
g_pui16EPISdram[RegBase + (15) << 1] = 0x05;
// 16 is send/received
g_pui16EPISdram[RegBase + (17) << 1] = 0x05;
g_pui16EPISdram[RegBase + (18) << 1] = 0x05;
g_pui16EPISdram[RegBase + (19) << 1] = 0x05;
g_pui16EPISdram[RegBase + (20) << 1] = 0x05;
g_pui16EPISdram[RegBase + (21) << 1] = 0x05;
g_pui16EPISdram[RegBase + (22) << 1] = 0x05;
g_pui16EPISdram[RegBase + (23) << 1] = 0x05;
// 24 is send/receive
g_pui16EPISdram[RegBase + (25) << 1] = 0x05;
g_pui16EPISdram[RegBase + (26) << 1] = 0x05;
g_pui16EPISdram[RegBase + (27) << 1] = 0x05;
g_pui16EPISdram[RegBase + (28) << 1] = 0x05;
g_pui16EPISdram[RegBase + (29) << 1] = 0x05;
g_pui16EPISdram[RegBase + (30) << 1] = 0x05;
g_pui16EPISdram[RegBase + (31) << 1] = 0x05;*/
}