Part Number: TMS570LS1224
Other Parts Discussed in Thread: HALCOGEN,
Tool/software: Code Composer Studio
Hi,
I've been having some trouble with an issue I can't really understand. I'm using Halcogen and CSS to create a program in which the TMS570LS1224 receives some messages via RX pin using interrupts. That seems to work well, but then I wanted to use some variable to keep track of how many messages the TMS570LS1224 receives, so I created a global value (declared outside any function) which I called j for this purpose. The problem is everytime I enter scinotification(), that variable somehow changes its value for seemingly no reason so it doesn't work as expected (it should be incremented by one everytime a new message is received). Can someone help me with this?
This is my code:
#include "sci.h"
#include "stdlib.h"
#include "sys_common.h"
static unsigned char npulses;
uint8_t j = 0;
int main(void)
{
_enable_IRQ();
sciInit();
sciReceive(sciREG,9,(unsigned char *)&npulses);
while(1);
}
void sciNotification(sciBASE_t *sci, unsigned flags)
{
j++;
sciSend(scilinREG, 9, (unsigned char *)&npulses);
sciReceive(sciREG,9,(unsigned char *)&npulses);
return;
}
void esmGroup1Notification(int bit)
{
return;
}
void esmGroup2Notification(int bit)
{
return;
}