Other Parts Discussed in Thread: TMS570LC4357,
Hi there,
Under MibSPI mode, while I understand the clarifications found in the TRM spnu499c, page 1397 for Last TG End Pointer programming in the case where all 8 TGs are been used, I cannot find what to do when all 128-element buffer are assigned to TG0 (or when less than 8 TGs are been used).
Should I simply set TG0 start pointer to 0 (as usual), then set LTGPEND-->LPEND end pointer to 127?
Or I need also configure TG1? If so, what start pointer value should I set for TG1, and what end pointer should I set for LPEND?
Thank you.