Part Number: TM4C1231E6PM
Tool/software: Code Composer Studio
We are developping a firmware with a bootloader (the firmware is loaded through UART1 peripheral).
Up to now we are creating two projects: one for only debug purpose and one to be loaded through UART1.
The reason is the following: if we try to load in debug mode a project that has the code enabling the bootloader, the program starts correctly but it blocks at random points. When I pause the debug, I observe the following message: No source available for "0xfffffffe" and looking in the "view Disassembly" the following message is shown: "???? Memory map prevented reading 0xFFFFFFFE [code=0x20000]".
The project with the the code enabling the bootloader is working correctly if it is loaded at the memory location 0x1000 using LMFLASH programmer (at location 0x0 I have to load before the bootloader).
The project without the code enabling the bootloader is working correctly both if it is loaded with LMFLASH Programmer and if it loaded in debug mode through Code Composer,
The project with the code enabling the bootloader has the following differences with respect to the "standard project":
1) Introduction of the routine
void
JumpToBootLoader(void)
{
//
// We must make sure we turn off SysTick and its interrupt before entering
// the boot loader!
//
ROM_SysTickIntDisable();
ROM_SysTickDisable();
//
// Disable all processor interrupts. Instead of disabling them
// one at a time, a direct write to NVIC is done to disable all
// peripheral interrupts.
//
HWREG(NVIC_DIS0) = 0xffffffff;
HWREG(NVIC_DIS1) = 0xffffffff;
HWREG(NVIC_DIS2) = 0xffffffff;
HWREG(NVIC_DIS3) = 0xffffffff;
HWREG(NVIC_DIS4) = 0xffffffff;
//
// Return control to the boot loader. This is a call to the SVC
// handler in the boot loader.
//
(*((void (*)(void))(*(uint32_t *)0x2c)))();
}
2) The routine UART1IntHandler has been modified in the following way
void
UART1IntHandler(void)
{
GPIO_PORTF_DATA_R &= ~ TX_EN_RS485;
uint32_t ui32StatusRX;
RingBufFlush(&rxRingBuf);
//
// Get the interrupt status.
//
ui32StatusRX = ROM_UARTIntStatus(UART1_BASE, true);
//
// Clear the asserted interrupts.
//
ROM_UARTIntClear(UART1_BASE, ui32StatusRX);
// The receive timeout interrupt fires when you have received bytes in your FIFO but have not
// gotten enough to fire your Rx interrupt. This is because the FIFO level select determines when that
// interrupt goes off.
if((ui32StatusRX & UART_INT_RT) == UART_INT_RT)
{
// While there are bytes to read and there is space in the FIFO.
while(UARTCharsAvail(UART1_BASE) && RingBufFull(&rxRingBuf) == false)
{
uint32_t ch = (uint8_t)ROM_UARTCharGet(UART1_BASE);
if(ch=='?')
{
GPIO_PORTF_DATA_R|=LED_GREEN;
GPIO_PORTF_DATA_R |= TX_EN_RS485;
UARTCharPut(UART1_BASE, 'B');
while(ROM_UARTBusy(UART1_BASE));
UARTCharPut(UART1_BASE, 'o');
while(ROM_UARTBusy(UART1_BASE));
UARTCharPut(UART1_BASE, 'o');
while(ROM_UARTBusy(UART1_BASE));
UARTCharPut(UART1_BASE, 't');
while(ROM_UARTBusy(UART1_BASE));
JumpToBootLoader();
}
// Write a byte straight from the hardware FIFO into our Rx FIFO for processing later.
RingBufWriteOne(&rxRingBuf, ch);
}
}
if((ui32StatusRX & UART_INT_RX) == UART_INT_RX)
{
//
// Loop while there are characters in the receive FIFO.
//
while(ROM_UARTCharsAvail(UART1_BASE) && RingBufFull(&rxRingBuf) == false)
{
//
// Read the next character from the UART
//
uint32_t ch = (uint8_t)ROM_UARTCharGet(UART1_BASE);
RingBufWriteOne(&rxRingBuf,ch);
}
}
}
3) In the file .cmd the address APP_BASE becomes 0x00001000 instead of 0x00000000
I am not an expert of bootloader but I guess that the issue is in the way in which the code is loaded through Code Composer.
Is there in Code Composer an option similar to "Program Address Offset" present in LMFlash Programmer?