Tool/software: Code Composer Studio
Tell me if I configured it correctly. I have two projects, CAN_TX and CAN_RX, this is CAN_RX.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Tool/software: Code Composer Studio
Tell me if I configured it correctly. I have two projects, CAN_TX and CAN_RX, this is CAN_RX.
Hello,
As i said in the thread from the link above:
"To use CAN Tx/Rx pin for sending/receiving CAN messages in HALCoGen-->CANn-->CANn Port tab, pins must be set as functional (CAN) from Tx/Rx Pin Mode Section. To use CAN Tx/Rx pins as GIO they must be set as GIO .
When CANn Tx/Rx pin is set as functional (CAN) then Direction, Pull up/down and open drain are not applicable."
And form TRM, Table 27-34