Part Number: TMS570LS3137
Other Parts Discussed in Thread: HALCOGEN,
Hi,
I have to test SRAM ECC logic in the controller. I am enabling SRAM ECC diagnostics in the startup code as below,
// Initialize memory
memoryInit(0x1U);
// Enable SRAM ECC
_coreEnableRamEcc_();
During run time, I have to inject SRAM ECC single bit error and need to check that RAM ECC correctable error is reported to ESM.
Below are the steps followed to inject a single bit error,
1. RAMOCUUR is cleared to 0
2. RAMTHRESHOLD is set as 1
3. ECC_WR_EN bit in TCRAM Module Control Register (RAMCTRL) is enabled.
After that,I am trying to flip a single bit in RAM ECC location to inject an error, but the CPU gets aborted when I access RAM ECC location.
Reason for the abort as read from DFSR is below,
Data Fault status register - 0x0000080D ( Write access permission failed?)
Please let me know why CPU gets aborted when writing to RAM ECC location ?