Part Number: TMS570LS0714
Other Parts Discussed in Thread: HALCOGEN
Hi,
I try to use the function 'SL_SelfTest_ADC()' of the SafeTI Diagnostic Library to test a ADC input pin,
but sometimes I get the result 'ADC_PIN_UNDETERMINED' because the ADC conversion value 'Vu' it lower than 'Vn' value,
which mean the ADC sample the input channel with SELF_TEST=1 and HILO=1, the result is lower than SELF_TEST=0.
Here is the ADC value when it perform the self testing.
I find there is a similar question in the forum, but no answer about it.
Regards,
Snaku