Other Parts Discussed in Thread: EK-TM4C123GXL
Hello,
I am a student currently taking an Embedded Systems course, and as part of my final project, I need to create a USB keyboard. I've found the standard example for the dk-tm4c123g board and have modified it to fit my board in much the same fashion as many others have already. However, I find that upon running, nothing is printed to the terminal after "Waiting for host...", because the program remains stuck in the "while(!g_bConnected){}" loop. It does not go to FaultISR or anything like that. I believe this is because my PC does not recognize my device as a USB device at all. I thought this could be an issue with installing the driver, so tried to do it manually from the windows-drivers folder, only to have Windows insist that it had the most up-to-date version already. I tried connecting the board the way it is described in the TM4C123G LaunchPad Workshop, Lab 7 using the usb_dev_bulk example to switch the connection from Debug to Device mode, but this didn't change anything. It seems to me that there's something very elementary that I'm missing. I'm quite new to the ways of USB, so would appreciate any help I can get.
Please find the code I am using below. The file "usb_keyb_structs.h" is exactly as found in the dk-tm4c123g example. I am using CCS version 9.1.0 if this helps.
Thank you
Sana
//*****************************************************************************
//
// usb_dev_keyboard.c - Main routines for the keyboard example.
//
// Copyright (c) 2011-2017 Texas Instruments Incorporated. All rights reserved.
// Software License Agreement
//
// Texas Instruments (TI) is supplying this software for use solely and
// exclusively on TI's microcontroller products. The software is owned by
// TI and/or its suppliers, and is protected under applicable copyright
// laws. You may not combine this software with "viral" open-source
// software in order to form a larger program.
//
// THIS SOFTWARE IS PROVIDED "AS IS" AND WITH ALL FAULTS.
// NO WARRANTIES, WHETHER EXPRESS, IMPLIED OR STATUTORY, INCLUDING, BUT
// NOT LIMITED TO, IMPLIED WARRANTIES OF MERCHANTABILITY AND FITNESS FOR
// A PARTICULAR PURPOSE APPLY TO THIS SOFTWARE. TI SHALL NOT, UNDER ANY
// CIRCUMSTANCES, BE LIABLE FOR SPECIAL, INCIDENTAL, OR CONSEQUENTIAL
// DAMAGES, FOR ANY REASON WHATSOEVER.
//
// This is part of revision 2.1.4.178 of the DK-TM4C123G Firmware Package.
//
//*****************************************************************************
#include <stdbool.h>
#include <stdint.h>
#include "driverlib/uart.h"
#include "driverlib/rom.h"
#include "inc/hw_memmap.h"
#include "inc/hw_types.h"
#include "inc/hw_gpio.h"
#include "inc/hw_sysctl.h"
#include "driverlib/debug.h"
#include "driverlib/fpu.h"
#include "driverlib/gpio.h"
#include "driverlib/pin_map.h"
#include "driverlib/sysctl.h"
#include "driverlib/systick.h"
#include "utils/uartstdio.h"
#include "usblib/usblib.h"
#include "usblib/usbhid.h"
#include "usblib/device/usbdevice.h"
#include "usblib/device/usbdhid.h"
#include "usblib/device/usbdhidkeyb.h"
#include "usb_keyb_structs.h"
#include "drivers/buttons.h"
#include <inc/tm4c123gh6pm.h>
//*****************************************************************************
//
//! \addtogroup example_list
//! <h1>USB HID Keyboard Device (usb_dev_keyboard)</h1>
//!
//! This example application turns the evaluation board into a USB keyboard
//! supporting the Human Interface Device class. When the push button is
//! pressed, a sequence of key presses is simulated to type a string. Care
//! should be taken to ensure that the active window can safely receive the
//! text; enter is not pressed at any point so no actions are attempted by the
//! host if a terminal window is used (for example). The status LED is used to
//! indicate the current Caps Lock state and is updated in response to any
//! other keyboard attached to the same USB host system.
//!
//! The device implemented by this application also supports USB remote wakeup
//! allowing it to request the host to reactivate a suspended bus. If the bus
//! is suspended (as indicated on the application display), pressing the
//! push button will request a remote wakeup assuming the host has not
//! specifically disabled such requests.
//
//*****************************************************************************
//*****************************************************************************
//
// The system tick timer period.
//
//*****************************************************************************
#define SYSTICKS_PER_SECOND 100
//*****************************************************************************
//
// A mapping from the ASCII value received from the UART to the corresponding
// USB HID usage code.
//
//*****************************************************************************
static const int8_t g_ppi8KeyUsageCodes[][2] =
{
{ 0, HID_KEYB_USAGE_SPACE }, // 0x20
{ HID_KEYB_LEFT_SHIFT, HID_KEYB_USAGE_1 }, // ! 0x21
{ HID_KEYB_LEFT_SHIFT, HID_KEYB_USAGE_FQUOTE }, // " 0x22
{ HID_KEYB_LEFT_SHIFT, HID_KEYB_USAGE_3 }, // # 0x23
{ HID_KEYB_LEFT_SHIFT, HID_KEYB_USAGE_4 }, // $ 0x24
{ HID_KEYB_LEFT_SHIFT, HID_KEYB_USAGE_5 }, // % 0x25
{ HID_KEYB_LEFT_SHIFT, HID_KEYB_USAGE_7 }, // & 0x26
{ 0, HID_KEYB_USAGE_FQUOTE }, // ' 0x27
{ HID_KEYB_LEFT_SHIFT, HID_KEYB_USAGE_9 }, // ( 0x28
{ HID_KEYB_LEFT_SHIFT, HID_KEYB_USAGE_0 }, // ) 0x29
{ HID_KEYB_LEFT_SHIFT, HID_KEYB_USAGE_8 }, // * 0x2a
{ HID_KEYB_LEFT_SHIFT, HID_KEYB_USAGE_EQUAL }, // + 0x2b
{ 0, HID_KEYB_USAGE_COMMA }, // , 0x2c
{ 0, HID_KEYB_USAGE_MINUS }, // - 0x2d
{ 0, HID_KEYB_USAGE_PERIOD }, // . 0x2e
{ 0, HID_KEYB_USAGE_FSLASH }, // / 0x2f
{ 0, HID_KEYB_USAGE_0 }, // 0 0x30
{ 0, HID_KEYB_USAGE_1 }, // 1 0x31
{ 0, HID_KEYB_USAGE_2 }, // 2 0x32
{ 0, HID_KEYB_USAGE_3 }, // 3 0x33
{ 0, HID_KEYB_USAGE_4 }, // 4 0x34
{ 0, HID_KEYB_USAGE_5 }, // 5 0x35
{ 0, HID_KEYB_USAGE_6 }, // 6 0x36
{ 0, HID_KEYB_USAGE_7 }, // 7 0x37
{ 0, HID_KEYB_USAGE_8 }, // 8 0x38
{ 0, HID_KEYB_USAGE_9 }, // 9 0x39
{ HID_KEYB_LEFT_SHIFT, HID_KEYB_USAGE_SEMICOLON }, // : 0x3a
{ 0, HID_KEYB_USAGE_SEMICOLON }, // ; 0x3b
{ HID_KEYB_LEFT_SHIFT, HID_KEYB_USAGE_COMMA }, // < 0x3c
{ 0, HID_KEYB_USAGE_EQUAL }, // = 0x3d
{ HID_KEYB_LEFT_SHIFT, HID_KEYB_USAGE_PERIOD }, // > 0x3e
{ HID_KEYB_LEFT_SHIFT, HID_KEYB_USAGE_FSLASH }, // ? 0x3f
{ HID_KEYB_LEFT_SHIFT, HID_KEYB_USAGE_2 }, // @ 0x40
{ HID_KEYB_LEFT_SHIFT, HID_KEYB_USAGE_A }, // A 0x41
{ HID_KEYB_LEFT_SHIFT, HID_KEYB_USAGE_B }, // B 0x42
{ HID_KEYB_LEFT_SHIFT, HID_KEYB_USAGE_C }, // C 0x43
{ HID_KEYB_LEFT_SHIFT, HID_KEYB_USAGE_D }, // D 0x44
{ HID_KEYB_LEFT_SHIFT, HID_KEYB_USAGE_E }, // E 0x45
{ HID_KEYB_LEFT_SHIFT, HID_KEYB_USAGE_F }, // F 0x46
{ HID_KEYB_LEFT_SHIFT, HID_KEYB_USAGE_G }, // G 0x47
{ HID_KEYB_LEFT_SHIFT, HID_KEYB_USAGE_H }, // H 0x48
{ HID_KEYB_LEFT_SHIFT, HID_KEYB_USAGE_I }, // I 0x49
{ HID_KEYB_LEFT_SHIFT, HID_KEYB_USAGE_J }, // J 0x4a
{ HID_KEYB_LEFT_SHIFT, HID_KEYB_USAGE_K }, // K 0x4b
{ HID_KEYB_LEFT_SHIFT, HID_KEYB_USAGE_L }, // L 0x4c
{ HID_KEYB_LEFT_SHIFT, HID_KEYB_USAGE_M }, // M 0x4d
{ HID_KEYB_LEFT_SHIFT, HID_KEYB_USAGE_N }, // N 0x4e
{ HID_KEYB_LEFT_SHIFT, HID_KEYB_USAGE_O }, // O 0x4f
{ HID_KEYB_LEFT_SHIFT, HID_KEYB_USAGE_P }, // P 0x50
{ HID_KEYB_LEFT_SHIFT, HID_KEYB_USAGE_Q }, // Q 0x51
{ HID_KEYB_LEFT_SHIFT, HID_KEYB_USAGE_R }, // R 0x52
{ HID_KEYB_LEFT_SHIFT, HID_KEYB_USAGE_S }, // S 0x53
{ HID_KEYB_LEFT_SHIFT, HID_KEYB_USAGE_T }, // T 0x54
{ HID_KEYB_LEFT_SHIFT, HID_KEYB_USAGE_U }, // U 0x55
{ HID_KEYB_LEFT_SHIFT, HID_KEYB_USAGE_V }, // V 0x56
{ HID_KEYB_LEFT_SHIFT, HID_KEYB_USAGE_W }, // W 0x57
{ HID_KEYB_LEFT_SHIFT, HID_KEYB_USAGE_X }, // X 0x58
{ HID_KEYB_LEFT_SHIFT, HID_KEYB_USAGE_Y }, // Y 0x59
{ HID_KEYB_LEFT_SHIFT, HID_KEYB_USAGE_Z }, // Z 0x5a
{ 0, HID_KEYB_USAGE_LBRACKET }, // [ 0x5b
{ 0, HID_KEYB_USAGE_BSLASH }, // \ 0x5c
{ 0, HID_KEYB_USAGE_RBRACKET }, // ] 0x5d
{ HID_KEYB_LEFT_SHIFT, HID_KEYB_USAGE_6 }, // ^ 0x5e
{ HID_KEYB_LEFT_SHIFT, HID_KEYB_USAGE_MINUS }, // _ 0x5f
{ 0, HID_KEYB_USAGE_BQUOTE }, // ` 0x60
{ 0, HID_KEYB_USAGE_A }, // a 0x61
{ 0, HID_KEYB_USAGE_B }, // b 0x62
{ 0, HID_KEYB_USAGE_C }, // c 0x63
{ 0, HID_KEYB_USAGE_D }, // d 0x64
{ 0, HID_KEYB_USAGE_E }, // e 0x65
{ 0, HID_KEYB_USAGE_F }, // f 0x66
{ 0, HID_KEYB_USAGE_G }, // g 0x67
{ 0, HID_KEYB_USAGE_H }, // h 0x68
{ 0, HID_KEYB_USAGE_I }, // i 0x69
{ 0, HID_KEYB_USAGE_J }, // j 0x6a
{ 0, HID_KEYB_USAGE_K }, // k 0x6b
{ 0, HID_KEYB_USAGE_L }, // l 0x6c
{ 0, HID_KEYB_USAGE_M }, // m 0x6d
{ 0, HID_KEYB_USAGE_N }, // n 0x6e
{ 0, HID_KEYB_USAGE_O }, // o 0x6f
{ 0, HID_KEYB_USAGE_P }, // p 0x70
{ 0, HID_KEYB_USAGE_Q }, // q 0x71
{ 0, HID_KEYB_USAGE_R }, // r 0x72
{ 0, HID_KEYB_USAGE_S }, // s 0x73
{ 0, HID_KEYB_USAGE_T }, // t 0x74
{ 0, HID_KEYB_USAGE_U }, // u 0x75
{ 0, HID_KEYB_USAGE_V }, // v 0x76
{ 0, HID_KEYB_USAGE_W }, // w 0x77
{ 0, HID_KEYB_USAGE_X }, // x 0x78
{ 0, HID_KEYB_USAGE_Y }, // y 0x79
{ 0, HID_KEYB_USAGE_Z }, // z 0x7a
{ HID_KEYB_LEFT_SHIFT, HID_KEYB_USAGE_LBRACKET }, // { 0x7b
{ HID_KEYB_LEFT_SHIFT, HID_KEYB_USAGE_BSLASH }, // | 0x7c
{ HID_KEYB_LEFT_SHIFT, HID_KEYB_USAGE_RBRACKET }, // } 0x7d
{ HID_KEYB_LEFT_SHIFT, HID_KEYB_USAGE_BQUOTE }, // ~ 0x7e
};
//*****************************************************************************
//
// This global indicates whether or not we are connected to a USB host.
//
//*****************************************************************************
volatile bool g_bConnected = false;
//*****************************************************************************
//
// This global indicates whether or not the USB bus is currently in the suspend
// state.
//
//*****************************************************************************
volatile bool g_bSuspended = false;
//*****************************************************************************
//
// Global system tick counter holds elapsed time since the application started
// expressed in 100ths of a second.
//
//*****************************************************************************
volatile uint32_t g_ui32SysTickCount;
//*****************************************************************************
//
// The number of system ticks to wait for each USB packet to be sent before
// we assume the host has disconnected. The value 50 equates to half a second.
//
//*****************************************************************************
#define MAX_SEND_DELAY 50
//*****************************************************************************
//
// This global is set to true if the host sends a request to set or clear
// any keyboard LED.
//
//*****************************************************************************
volatile bool g_bDisplayUpdateRequired;
//*****************************************************************************
//
// This enumeration holds the various states that the keyboard can be in during
// normal operation.
//
//*****************************************************************************
int keyBC = 0;
volatile enum
{
//
// Unconfigured.
//
STATE_UNCONFIGURED,
//
// No keys to send and not waiting on data.
//
STATE_IDLE,
//
// Waiting on data to be sent out.
//
STATE_SENDING
}
g_eKeyboardState = STATE_UNCONFIGURED;
//*****************************************************************************
//
// The error routine that is called if the driver library encounters an error.
//
//*****************************************************************************
#ifdef DEBUG
void
__error__(char *pcFilename, uint32_t ui32Line)
{
}
#endif
//*****************************************************************************
//
// Handles asynchronous events from the HID keyboard driver.
//
// \param pvCBData is the event callback pointer provided during
// USBDHIDKeyboardInit(). This is a pointer to our keyboard device structure
// (&g_sKeyboardDevice).
// \param ui32Event identifies the event we are being called back for.
// \param ui32MsgData is an event-specific value.
// \param pvMsgData is an event-specific pointer.
//
// This function is called by the HID keyboard driver to inform the application
// of particular asynchronous events related to operation of the keyboard HID
// device.
//
// \return Returns 0 in all cases.
//
//*****************************************************************************
uint32_t
KeyboardHandler(void *pvCBData, uint32_t ui32Event, uint32_t ui32MsgData,
void *pvMsgData)
{
keyBC=1;
switch (ui32Event)
{
//
// The host has connected to us and configured the device.
//
case USB_EVENT_CONNECTED:
{
g_bConnected = true;
g_bSuspended = false;
break;
}
//
// The host has disconnected from us.
//
case USB_EVENT_DISCONNECTED:
{
g_bConnected = false;
break;
}
//
// We receive this event every time the host acknowledges transmission
// of a report. It is used here purely as a way of determining whether
// the host is still talking to us or not.
//
case USB_EVENT_TX_COMPLETE:
{
//
// Enter the idle state since we finished sending something.
//
int i = 0;
g_eKeyboardState = STATE_IDLE;
for (; i < 100000; ++i)
{;}
break;
}
//
// This event indicates that the host has suspended the USB bus.
//
case USB_EVENT_SUSPEND:
{
g_bSuspended = true;
break;
}
//
// This event signals that the host has resumed signalling on the bus.
//
case USB_EVENT_RESUME:
{
g_bSuspended = false;
break;
}
//
// This event indicates that the host has sent us an Output or
// Feature report and that the report is now in the buffer we provided
// on the previous USBD_HID_EVENT_GET_REPORT_BUFFER callback.
//
case USBD_HID_KEYB_EVENT_SET_LEDS:
{
//
// Set the LED to match the current state of the caps lock LED.
//
ROM_GPIOPinWrite(GPIO_PORTF_BASE, GPIO_PIN_2,
(ui32MsgData & HID_KEYB_CAPS_LOCK) ? GPIO_PIN_2 :
0);
break;
}
//
// We ignore all other events.
//
default:
{
break;
}
}
return(0);
}
//***************************************************************************
//
// Wait for a period of time for the state to become idle.
//
// \param ui32TimeoutTick is the number of system ticks to wait before
// declaring a timeout and returning \b false.
//
// This function polls the current keyboard state for ui32TimeoutTicks system
// ticks waiting for it to become idle. If the state becomes idle, the
// function returns true. If it ui32TimeoutTicks occur prior to the state
// becoming idle, false is returned to indicate a timeout.
//
// \return Returns \b true on success or \b false on timeout.
//
//***************************************************************************
bool
WaitForSendIdle(uint_fast32_t ui32TimeoutTicks)
{
uint32_t ui32Start;
uint32_t ui32Now;
uint32_t ui32Elapsed;
ui32Start = g_ui32SysTickCount;
ui32Elapsed = 0;
while(ui32Elapsed < ui32TimeoutTicks)
{
//
// Is the keyboard is idle, return immediately.
//
if(g_eKeyboardState == STATE_IDLE)
{
return(true);
}
//
// Determine how much time has elapsed since we started waiting. This
// should be safe across a wrap of g_ui32SysTickCount.
//
ui32Now = g_ui32SysTickCount;
ui32Elapsed = ((ui32Start < ui32Now) ? (ui32Now - ui32Start) :
(((uint32_t)0xFFFFFFFF - ui32Start) + ui32Now + 1));
}
//
// If we get here, we timed out so return a bad return code to let the
// caller know.
//
return(false);
}
//*****************************************************************************
//
// Sends a string of characters via the USB HID keyboard interface.
//
//*****************************************************************************
void
SendString(char *pcStr)
{
uint32_t ui32Char;
//
// Loop while there are more characters in the string.
//
while(*pcStr)
{
//
// Get the next character from the string.
//
ui32Char = *pcStr++;
//
// Skip this character if it is a non-printable character.
//
if((ui32Char < ' ') || (ui32Char > '~'))
{
continue;
}
//
// Convert the character into an index into the keyboard usage code
// table.
//
ui32Char -= ' ';
//
// Send the key press message.
//
g_eKeyboardState = STATE_SENDING;
if(USBDHIDKeyboardKeyStateChange((void *)&g_sKeyboardDevice,
g_ppi8KeyUsageCodes[ui32Char][0],
g_ppi8KeyUsageCodes[ui32Char][1],
true) != KEYB_SUCCESS)
{
return;
}
//
// Wait until the key press message has been sent.
//
if(!WaitForSendIdle(MAX_SEND_DELAY))
{
g_bConnected = 0;
return;
}
//
// Send the key release message.
//
g_eKeyboardState = STATE_SENDING;
if(USBDHIDKeyboardKeyStateChange((void *)&g_sKeyboardDevice,
0, g_ppi8KeyUsageCodes[ui32Char][1],
false) != KEYB_SUCCESS)
{
return;
}
//
// Wait until the key release message has been sent.
//
if(!WaitForSendIdle(MAX_SEND_DELAY))
{
g_bConnected = 0;
return;
}
}
}
//*****************************************************************************
//
// This is the interrupt handler for the SysTick interrupt. It is used to
// update our local tick count which, in turn, is used to check for transmit
// timeouts.
//
//*****************************************************************************
void
SysTickIntHandler(void)
{
g_ui32SysTickCount++;
}
//*****************************************************************************
//
// Configure UART and its pins. This must be called before UARTprintf().
//
//*****************************************************************************
void
ConfigureUART(void)
{
//
// Enable the GPIO Peripheral used by the UART.
//
ROM_SysCtlPeripheralEnable(SYSCTL_PERIPH_GPIOA);
//
// Enable UART0
//
ROM_SysCtlPeripheralEnable(SYSCTL_PERIPH_UART0);
//
// Configure GPIO Pins for UART mode.
//
ROM_GPIOPinConfigure(GPIO_PA0_U0RX);
ROM_GPIOPinConfigure(GPIO_PA1_U0TX);
ROM_GPIOPinTypeUART(GPIO_PORTA_BASE, GPIO_PIN_0 | GPIO_PIN_1);
//
// Use the internal 16MHz oscillator as the UART clock source.
//
UARTClockSourceSet(UART0_BASE, UART_CLOCK_PIOSC);
//
// Initialize the UART for console I/O.
//
UARTStdioConfig(0, 115200, 16000000);
}
//*****************************************************************************
//
// This is the main loop that runs the application.
//
//*****************************************************************************
int
main(void)
{
uint_fast32_t ui32LastTickCount;
bool bLastSuspend;
// Enable lazy stacking for interrupt handlers. This allows floating-point
// instructions to be used within interrupt handlers, but at the expense of
// extra stack usage.
//
ROM_FPULazyStackingEnable();
//
// Set the clocking to run from the PLL at 50MHz.
//
ROM_SysCtlClockSet(SYSCTL_SYSDIV_4 | SYSCTL_USE_PLL | SYSCTL_OSC_MAIN |
SYSCTL_XTAL_16MHZ);
/* **************************************************************** */
// Enable the GPIO port that is used for the on-board LED.
//
ROM_SysCtlPeripheralEnable(SYSCTL_PERIPH_GPIOF);
//
// Enable the GPIO pin for the Blue LED (PF2).
//
ROM_GPIOPinTypeGPIOOutput(GPIO_PORTF_BASE, GPIO_PIN_2);
//
// Open UART0 and show the application name on the UART.
//
ConfigureUART();
UARTprintf("USB keyboard\n");
UARTprintf("---------------------------------\n\n");
// Enable the GPIO peripheral used for USB, and configure the USB
// pins.
//
ROM_SysCtlPeripheralEnable(SYSCTL_PERIPH_GPIOD);
SysCtlGPIOAHBEnable(SYSCTL_PERIPH_GPIOD);
ROM_GPIOPinTypeUSBAnalog(GPIO_PORTD_AHB_BASE, GPIO_PIN_4 | GPIO_PIN_5);
/* **************************************************************** */
//
// Erratum workaround for silicon revision A1. VBUS must have pull-down.
//
if(CLASS_IS_TM4C123 && REVISION_IS_A1)
{
HWREG(GPIO_PORTB_BASE + GPIO_O_PDR) |= GPIO_PIN_1;
}
// Initialize the buttons driver
//
ButtonsInit();
//
// Not configured initially.
//
g_bConnected = false;
g_bSuspended = false;
bLastSuspend = false;
//
// Initialize the USB stack for device mode.
//
USBStackModeSet(0, eUSBModeDevice, 0);
//
// Pass our device information to the USB HID device class driver,
// initialize the USB
// controller and connect the device to the bus.
//
USBDHIDKeyboardInit(0, &g_sKeyboardDevice);
//
// Set the system tick to fire 100 times per second.
//
ROM_SysTickPeriodSet(ROM_SysCtlClockGet() / SYSTICKS_PER_SECOND);
ROM_SysTickIntEnable();
ROM_SysTickEnable();
//
// The main loop starts here. We begin by waiting for a host connection
// then drop into the main keyboard handling section. If the host
// disconnects, we return to the top and wait for a new connection.
//
while(1)
{
uint8_t ui8Buttons;
uint8_t ui8ButtonsChanged;
UARTprintf("Waiting for host...\n");
while(!g_bConnected)
{
}
UARTprintf("Host connected...\n");
//
// Enter the idle state.
//
g_eKeyboardState = STATE_IDLE;
//
// Assume that the bus is not currently suspended if we have just been
// configured.
//
bLastSuspend = false;
//
// Keep transferring characters from the UART to the USB host for as
// long as we are connected to the host.
//
while(g_bConnected)
{
//
// Remember the current time.
//
ui32LastTickCount = g_ui32SysTickCount;
//
// Has the suspend state changed since last time we checked?
//
if(bLastSuspend != g_bSuspended)
{
//
// Yes - the state changed so update the display.
//
bLastSuspend = g_bSuspended;
if(bLastSuspend)
{
UARTprintf("\nBus Suspended...\n");
}
else
{
UARTprintf("\nHost Connected...\n");
}
}
//
// See if the button was just pressed.
//
ui8Buttons = ButtonsPoll(&ui8ButtonsChanged, 0);
if(BUTTON_PRESSED(LEFT_BUTTON, ui8Buttons, ui8ButtonsChanged))
{
//
// If the bus is suspended then resume it. Otherwise, type
// some "random" characters.
//
if(g_bSuspended)
{
USBDHIDKeyboardRemoteWakeupRequest(
(void *)&g_sKeyboardDevice);
}
else
{
SendString("Phew. \n");
}
}
while(g_ui32SysTickCount == ui32LastTickCount)
{
}
}
if(g_bConnected == false)
{
UARTprintf("Host disconnected...\n");
}
}
}