This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

EK-TM4C123GXL: [URGENT]Got problem with the implementation of PWM at portB7 of the EK-TM4C123GXL board.

Part Number: EK-TM4C123GXL

I'm using a EK-TM4C123GXL board to run a tower pro sg90 servo motor.My system clock is running at 16Mhz and im using Keil to program.Given below is the code I wrote, but there is no movement on the servo.

#include "tm4c123gh6pm.h"											//header file, tm4c123gh6pm register descriptions
/***************************************Definition************************************/
#define SIGNAL (01U << 7)											//PWM signal 
#define LOAD 		0x270FF												//LOAD value = 159,999
/***************************************************************************************/

void PWM_init()
//PWM_init function enables PWM at PortB7 to work in a countdown mode.
{
	SYSCTL_RCGC0_R |= SYSCTL_RCGC0_PWM0;				//Enable pwm clock
	SYSCTL_RCGC2_R |= SYSCTL_RCGC2_GPIOB;				//PORT B clock enable
	__asm{nop 
				nop}																	//Two NOP delay to stabilize clock (Mixed ASM C Programming)
	GPIO_PORTB_DIR_R |= SIGNAL;									//Set the B7 pin as output
	GPIO_PORTB_AFSEL_R |= SIGNAL;								//Enable Alternate function for B7
	GPIO_PORTB_PCTL_R &= ~(GPIO_PCTL_PB7_M);		//PORT mux control for PB7 - Clear bit
	GPIO_PORTB_PCTL_R |= GPIO_PCTL_PB7_M0PWM1;	//PORT mux control for PB7 - set PWM				
	GPIO_PORTB_DATA_R |= SIGNAL;								//Data enable for PB7
	SYSCTL_RCC_R |= SYSCTL_RCC_USEPWMDIV; 			//Enable PWM divider
	SYSCTL_RCC_R &= ~(SYSCTL_RCC_PWMDIV_M);			//Clear PWM divider filed
	SYSCTL_RCC_R |= SYSCTL_RCC_PWMDIV_2;				//Set PWM divide as /2
	PWM0_1_CTL_R = 0x00000000;									//Disable PWM timer

	//Masking the action for Bdown & counter = LOAD
	PWM0_1_GENB_R &=~(PWM_0_GENB_ACTCMPBD_M | PWM_0_GENB_ACTLOAD_M);
	PWM0_1_GENB_R |= (PWM_0_GENB_ACTLOAD_ONE | PWM_0_GENB_ACTCMPBD_ZERO);
				
	PWM0_1_LOAD_R = LOAD;												//LOAD value set as 159,999
	PWM0_1_CMPB_R = LOAD*(0.9);									//Initial value for comparator B is 0.9*LOAD
	PWM0_1_CTL_R = PWM_0_CTL_ENABLE;						//Enable PWM timer
	PWM0_ENABLE_R = PWM_ENABLE_PWM1EN;					//Enable PWM
}

int main()
{
	PWM_init();
}

Please can somebody tell me whats wrong in the code?