Part Number: TM4C123GE6PM
Tool/software: Code Composer Studio
Hi
i am have written I2C code to read TCS34725 devcie ID and able to send command and receive response but in my response i am getting only read address response not the next byte below is my code and response attached i need to read 2 byte response but i read only 1 byte please let me know what i have missed
//*****************************************************************************
//
// slave_receive_int.c - Example demonstrating a simple I2C master message
// transmission using a slave interrupt when data is
// received.
//
// Copyright (c) 2010-2015 Texas Instruments Incorporated. All rights reserved.
// Software License Agreement
//
// Redistribution and use in source and binary forms, with or without
// modification, are permitted provided that the following conditions
// are met:
//
// Redistributions of source code must retain the above copyright
// notice, this list of conditions and the following disclaimer.
//
// Redistributions in binary form must reproduce the above copyright
// notice, this list of conditions and the following disclaimer in the
// documentation and/or other materials provided with the
// distribution.
//
// Neither the name of Texas Instruments Incorporated nor the names of
// its contributors may be used to endorse or promote products derived
// from this software without specific prior written permission.
//
// THIS SOFTWARE IS PROVIDED BY THE COPYRIGHT HOLDERS AND CONTRIBUTORS
// "AS IS" AND ANY EXPRESS OR IMPLIED WARRANTIES, INCLUDING, BUT NOT
// LIMITED TO, THE IMPLIED WARRANTIES OF MERCHANTABILITY AND FITNESS FOR
// A PARTICULAR PURPOSE ARE DISCLAIMED. IN NO EVENT SHALL THE COPYRIGHT
// OWNER OR CONTRIBUTORS BE LIABLE FOR ANY DIRECT, INDIRECT, INCIDENTAL,
// SPECIAL, EXEMPLARY, OR CONSEQUENTIAL DAMAGES (INCLUDING, BUT NOT
// LIMITED TO, PROCUREMENT OF SUBSTITUTE GOODS OR SERVICES; LOSS OF USE,
// DATA, OR PROFITS; OR BUSINESS INTERRUPTION) HOWEVER CAUSED AND ON ANY
// THEORY OF LIABILITY, WHETHER IN CONTRACT, STRICT LIABILITY, OR TORT
// (INCLUDING NEGLIGENCE OR OTHERWISE) ARISING IN ANY WAY OUT OF THE USE
// OF THIS SOFTWARE, EVEN IF ADVISED OF THE POSSIBILITY OF SUCH DAMAGE.
//
// This is part of revision 2.1.1.71 of the Tiva Firmware Development Package.
//
//*****************************************************************************
#include <stdbool.h>
#include <stdint.h>
#include "inc/hw_i2c.h"
#include "inc/hw_ints.h"
#include "inc/hw_memmap.h"
#include "inc/hw_types.h"
#include "driverlib/gpio.h"
#include "driverlib/i2c.h"
#include "driverlib/interrupt.h"
#include "driverlib/pin_map.h"
#include "driverlib/sysctl.h"
#include "driverlib/uart.h"
#include "utils/uartstdio.h"
uint32_t I2CReceive(uint32_t slave_addr, uint8_t reg);
//*****************************************************************************
//
//! \addtogroup i2c_examples_list
//! <h1>Slave Receive Interrupt (slave_receive_int)</h1>
//!
//! This example shows how to configure a receive interrupt on the slave
//! module. This includes setting up the I2C0 module for loopback mode as well
//! as configuring the master and slave modules. Loopback mode internally
//! connects the master and slave data and clock lines together. The address
//! of the slave module is set to a value so it can receive data from the
//! master.
//!
//! This example uses the following peripherals and I/O signals. You must
//! review these and change as needed for your own board:
//! - I2C0 peripheral
//! - GPIO Port B peripheral (for I2C0 pins)
//! - I2C0SCL - PB2
//! - I2C0SDA - PB3
//!
//! The following UART signals are configured only for displaying console
//! messages for this example. These are not required for operation of I2C.
//! - UART0 peripheral
//! - GPIO Port A peripheral (for UART0 pins)
//! - UART0RX - PA0
//! - UART0TX - PA1
//!
//! This example uses the following interrupt handlers. To use this example
//! in your own application you must add these interrupt handlers to your
//! vector table.
//! - INT_I2C0 - I2C0SlaveIntHandler
//
//*****************************************************************************
//*****************************************************************************
//
// Set the address for slave module. This is a 7-bit address sent in the
// following format:
// [A6:A5:A4:A3:A2:A1:A0:RS]
//
// A zero in the R/S position of the first byte means that the master
// transmits (sends) data to the selected slave, and a one in this position
// means that the master receives data from the slave.
//
//*****************************************************************************
#define SLAVE_ADDRESS 0x29
//*****************************************************************************
//
// Global variable to hold the I2C data that has been received.
//
//*****************************************************************************
static uint32_t g_ui32DataRx1;
static uint32_t g_ui32DataRx2;
static uint32_t g_ui32DataRx3;
static uint32_t data_count=2;
//*****************************************************************************
//
// This is a flag that gets set in the interrupt handler to indicate that an
// interrupt occurred.
//
//*****************************************************************************
static bool g_bIntFlag = false;
//*****************************************************************************
//
// This function sets up UART0 to be used for a console to display information
// as the example is running.
//
//*****************************************************************************
void
InitConsole(void)
{
//
// Enable GPIO port A which is used for UART0 pins.
// TODO: change this to whichever GPIO port you are using.
//
SysCtlPeripheralEnable(SYSCTL_PERIPH_GPIOA);
//
// Configure the pin muxing for UART0 functions on port A0 and A1.
// This step is not necessary if your part does not support pin muxing.
// TODO: change this to select the port/pin you are using.
//
GPIOPinConfigure(GPIO_PA0_U0RX);
GPIOPinConfigure(GPIO_PA1_U0TX);
//
// Enable UART0 so that we can configure the clock.
//
SysCtlPeripheralEnable(SYSCTL_PERIPH_UART0);
//
// Use the internal 16MHz oscillator as the UART clock source.
//
UARTClockSourceSet(UART0_BASE, UART_CLOCK_PIOSC);
//
// Select the alternate (UART) function for these pins.
// TODO: change this to select the port/pin you are using.
//
GPIOPinTypeUART(GPIO_PORTA_BASE, GPIO_PIN_0 | GPIO_PIN_1);
//
// Initialize the UART for console I/O.
//
UARTStdioConfig(0, 115200, 16000000);
}
//*****************************************************************************
//
// The interrupt handler for the for I2C0 data slave interrupt.
//
//*****************************************************************************
void I2C0SlaveIntHandler(void)
{
//
// Clear the I2C0 interrupt flag.
//
I2CSlaveIntClear(I2C0_BASE);
//
// Read the data from the slave.
//
g_ui32DataRx1= I2CSlaveDataGet(I2C0_BASE);
//
// Set a flag to indicate that the interrupt occurred.
//
g_bIntFlag = true;
}
//*****************************************************************************
//
// Configure the I2C0 master and slave and connect them using loopback mode.
//
//*****************************************************************************
int
main(void)
{
#if defined(TARGET_IS_TM4C129_RA0) || \
defined(TARGET_IS_TM4C129_RA1) || \
defined(TARGET_IS_TM4C129_RA2)
uint32_t ui32SysClock;
#endif
uint32_t ui32DataTx[3];
//
// Set the clocking to run directly from the external crystal/oscillator.
// TODO: The SYSCTL_XTAL_ value must be changed to match the value of the
// crystal on your board.
//
#if defined(TARGET_IS_TM4C129_RA0) || \
defined(TARGET_IS_TM4C129_RA1) || \
defined(TARGET_IS_TM4C129_RA2)
ui32SysClock = SysCtlClockFreqSet((SYSCTL_XTAL_25MHZ |
SYSCTL_OSC_MAIN |
SYSCTL_USE_PLL), 25000000);
#else
SysCtlClockSet(SYSCTL_SYSDIV_1 | SYSCTL_USE_OSC | SYSCTL_OSC_MAIN |
SYSCTL_XTAL_16MHZ);
#endif
//
// The I2C0 peripheral must be enabled before use.
//
SysCtlPeripheralEnable(SYSCTL_PERIPH_I2C0);
//
// For this example I2C0 is used with PortB[3:2]. The actual port and
// pins used may be different on your part, consult the data sheet for
// more information. GPIO port B needs to be enabled so these pins can
// be used.
// TODO: change this to whichever GPIO port you are using.
//
SysCtlPeripheralEnable(SYSCTL_PERIPH_GPIOB);
//
// Configure the pin muxing for I2C0 functions on port B2 and B3.
// This step is not necessary if your part does not support pin muxing.
// TODO: change this to select the port/pin you are using.
//
GPIOPinConfigure(GPIO_PB2_I2C0SCL);
GPIOPinConfigure(GPIO_PB3_I2C0SDA);
//
// Select the I2C function for these pins. This function will also
// configure the GPIO pins pins for I2C operation, setting them to
// open-drain operation with weak pull-ups. Consult the data sheet
// to see which functions are allocated per pin.
// TODO: change this to select the port/pin you are using.
//
GPIOPinTypeI2CSCL(GPIO_PORTB_BASE, GPIO_PIN_2);
GPIOPinTypeI2C(GPIO_PORTB_BASE, GPIO_PIN_3);
//
// Enable loopback mode. Loopback mode is a built in feature that helps
// for debug the I2Cx module. It internally connects the I2C master and
// slave terminals, which effectively lets you send data as a master and
// receive data as a slave. NOTE: For external I2C operation you will need
// to use external pull-ups that are faster than the internal pull-ups.
// Refer to the datasheet for more information.
//
HWREG(I2C0_BASE + I2C_O_MCR) |= 0x01;
//
// Enable the I2C0 interrupt on the processor (NVIC).
//
IntEnable(INT_I2C0);
//
// Configure and turn on the I2C0 slave interrupt. The I2CSlaveIntEnableEx()
// gives you the ability to only enable specific interrupts. For this case
// we are only interrupting when the slave device receives data.
//
I2CSlaveIntEnableEx(I2C0_BASE, I2C_SLAVE_INT_DATA);
//
// Enable and initialize the I2C0 master module. Use the system clock for
// the I2C0 module. The last parameter sets the I2C data transfer rate.
// If false the data rate is set to 100kbps and if true the data rate will
// be set to 400kbps. For this example we will use a data rate of 100kbps.
//
#if defined(TARGET_IS_TM4C129_RA0) || \
defined(TARGET_IS_TM4C129_RA1) || \
defined(TARGET_IS_TM4C129_RA2)
I2CMasterInitExpClk(I2C0_BASE, ui32SysClock, false);
#else
I2CMasterInitExpClk(I2C0_BASE, SysCtlClockGet(), false);
#endif
//
// Enable the I2C0 slave module.
//
I2CSlaveEnable(I2C0_BASE);
//
// Set the slave address to SLAVE_ADDRESS. In loopback mode, it's an
// arbitrary 7-bit number (set in a macro above) that is sent to the
// I2CMasterSlaveAddrSet function.
//
I2CSlaveInit(I2C0_BASE, SLAVE_ADDRESS);
//
// Tell the master module what address it will place on the bus when
// communicating with the slave. Set the address to SLAVE_ADDRESS
// (as set in the slave module). The receive parameter is set to false
// which indicates the I2C Master is initiating a writes to the slave. If
// true, that would indicate that the I2C Master is initiating reads from
// the slave.
//
I2CMasterSlaveAddrSet(I2C0_BASE, SLAVE_ADDRESS, false);
//
// Set up the serial console to use for displaying messages. This is just
// for this example program and is not needed for proper I2C operation.
//
InitConsole();
//
// Enable interrupts to the processor.
//
// IntMasterEnable();
//
// Display the example setup on the console.
//
UARTprintf("I2C Slave Interrupt Example ->");
UARTprintf("\n Module = I2C0");
UARTprintf("\n Mode = Receive interrupt on the Slave module");
UARTprintf("\n Rate = 100kbps\n\n");
//
// Initialize the data to send.
//
ui32DataTx[0] = 0x00;
ui32DataTx[1] = 0x01;
ui32DataTx[2] = 0x12;
while(1)
{
UARTprintf("Transferring from: Master -> Slave\n");
UARTprintf(" Sending: '%x'", ui32DataTx[0]);
I2CMasterDataPut(I2C0_BASE, ui32DataTx[0]);
I2CMasterControl(I2C0_BASE, I2C_MASTER_CMD_SINGLE_SEND);
while(!I2CMasterBusy(I2C0_BASE));
UARTprintf("Transferring from: Master -> Slave\n");
UARTprintf(" Sending: '%x'", ui32DataTx[1]);
I2CMasterDataPut(I2C0_BASE, ui32DataTx[1]);
I2CMasterControl(I2C0_BASE, I2C_MASTER_CMD_SINGLE_SEND);
while(!I2CMasterBusy(I2C0_BASE));
SysCtlDelay(1000000);
UARTprintf("Transferring from: Master -> Slave\n");
UARTprintf(" Sending: '%x'", ui32DataTx[2]);
I2CMasterDataPut(I2C0_BASE, ui32DataTx[2]);
I2CMasterControl(I2C0_BASE, I2C_MASTER_CMD_SINGLE_SEND);
I2CMasterSlaveAddrSet(I2C0_BASE, SLAVE_ADDRESS, true);
I2CMasterControl(I2C0_BASE, I2C_MASTER_CMD_BURST_RECEIVE_START);
while(!I2CMasterBusy(I2C0_BASE));
g_ui32DataRx1 = (uint8_t)I2CMasterDataGet(I2C0_BASE);
while(!I2CMasterBusy(I2C0_BASE));
I2CMasterControl(I2C0_BASE, I2C_MASTER_CMD_BURST_SEND_CONT);
g_ui32DataRx2 = (uint8_t)I2CMasterDataGet(I2C0_BASE);
I2CMasterControl(I2C0_BASE, I2C_MASTER_CMD_BURST_RECEIVE_FINISH);
while(!I2CMasterBusy(I2C0_BASE));
g_ui32DataRx3= (uint8_t)I2CMasterDataGet(I2C0_BASE);
I2CMasterControl(I2C0_BASE, I2C_MASTER_CMD_BURST_SEND_FINISH);
UARTprintf("\n Slave Interrupt Received!\n");
UARTprintf(" Received: '%x'\n\n", g_ui32DataRx1);
UARTprintf(" Received: '%x'\n\n", g_ui32DataRx2);
UARTprintf(" Received: '%x'\n\n", g_ui32DataRx3);
SysCtlDelay(10000000);
}
}
RESPONSE FROM UART TERMINAL
I2C Slave Interrupt Example ->
Module = I2C0
Mode = Receive interrupt on the Slave module
Rate = 100kbps
Transferring from: Master -> Slave
Sending: '0'Transferring from: Master -> Slave
Sending: '1'Transferring from: Master -> Slave
Sending: '12'
Slave Interrupt Received!
Received: '53' /// address os 0x29 lead to 0x53 of read
Received: '0'
Received: '0'