This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Tool/software: Code Composer Studio
Hi, Ti friends,
We have been using RM44L520 in our projects for more than 2 years. It works well.
But recently we have a problem with one of our board (only occurs on this board): One day, we just found that we could not upload program to the RM44L520 anymore. We could do this before. And the same program can be uploaded to other RM44L520s using the same PC and XDS.
In CCS it shows:
CortexR4: GEL Output: Memory Map Setup for Flash @ Address 0x0CortexR4: GEL Output: Memory Map Setup for Flash @ Address 0x0 due to System Reset
CortexR4: File Loader: Memory write failed: Algorithm indicated it failed to erase bank 0, sector 0
CortexR4: GEL: File: E:\YS\SW\02_PRJ\03_VA21\07_code\int\sr_emb\sr_safeguard_top\Release\sr_safeguard_top.out: Load failed.
CortexR4: GEL Output: Memory Map Setup for Flash @ Address 0x0 due to System Reset
We tried to erase any sector of the flash by using Uniflash. but failed;
And we also tried to read the contents out of the flash. It works; Besides, the program stored before can still work after power on (it flashes a 7 segment display).
We have searched the E2E forum for possible clues, but so far our problem is still unsolved.
Hi,QJ,
Thank you for the replying.
If possible, could you pls share more info about this damage? like possible root causes for this kind of damage?
We have already a protecting circuit for this JTAG interface. Maybe that's still not enough?
Many thanks.
Best regards from
AL Tang
Hello Tang,
The over voltage (>4.6V) on VCCP power supply pin will damage the circuitry of the flash pump.