Part Number: TMS570LS1227
Hi team,
My customer now finds a issue that TMS570 occasionally(during several days stability experiment) will encounter a issue that the UART TX has no output(voltage level is high or low is not recorded).
This uart(UART1) interfaces to a level shift chip then a 4G module, and another uart(UART2) is used to print out log. Occasionally UART1 TX will have no output(tested by oscilloscope) while the UART2 printed log indicates the APP is still running. Normally UART1 TX should output a package every 600ms.
They wonder what may cause the TX have no output? Power down and up the device then everything goes back to normal.
Thanks
Gary