Part Number: TMS570LC4357
Tool/software: Code Composer Studio
Hi,
I am Using TMS570LC4357 for my project and I have connected the RS422( MAX3488EESA ) Tx and Rx to SCI Tx and Rx Respectively.
When i am doing the external loopback for this connection then i can able to transmit and receive the data properly.
If i attached the RS422 to serial connector and tries to send the data from Other PC to processor then I am unable to receive the data accurately.
Although, to check the Serial Converter, i also tested that for loopback, there also i could not find any problem.
I Probed the pins for the reception, there i could able to get the proper data, but in the register i cannot see the same.
It is like when i am transmitting the 0x31 i should get it same. But, I am receiving the data as 0xE3.
Can Anyone please help me in understanding this behaviour.
Regards,
Shivam Kakad