This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Compiler/TMS570LS3137: when the cpu is Self-checking,What is the status of the CPU

Part Number: TMS570LS3137

Tool/software: TI C/C++ Compiler

 Hi

 TMS570LS3137 CPU is self-checking,  I see "SafeTI™ Hercules™ Diagnostic Library Release version 2.3.2"paper,some api spend more time.

 question:

 1.if cpu is self-checking ,Whether the interrupt function can execute.

2.The CPU self-test takes a long time, which will affect the operation of the entire program and the real-time response?

  Thanks

  

   

  • Hello,

    1. No, the CPU core master bus transaction signals are configured to be in idle mode during the self-test tun.

    2. You can run the STC test during startup or can divide STC into 24 or fewer intervals and run them during normal operation. If STC is divided into intervals and ran, user software must save the CPU contents and reload them after the CPU reset caused by the completion of the STC test interval.

    It only takes 1365 clock cycles (15.17 us at VCLK=90MHz) for each test interval.

  • Thank you 

    During the self-test tun,cpu can't do anything ,which is very scary thing.

    what does this means, take long time?

     

  • Thank you 

    During the self-test tun,cpu can't do anything ,which is very scary thing.

    what does this means, take long time?

     

  • Hello

     I want to know this api function ..""

      when those api function run,can the cpu  run the other interrupt function?

  • Hello,

    The PBIST is usually run on device start-up as it is a destructive test and all contents of the tested SRAM module are overwritten during the test. 

    During CPU selftest, the CPU core is completely isolated from the rest of the system. After CPU selftest, the STC generates a CPU reset regardless of pass of fail of the test. 

    CPU will not handle the interrupts during those 2 selftests.