Part Number: TMS570LC4357
Other Parts Discussed in Thread: DP83640, HALCOGEN, CCSTUDIO
Hello,
i'm trying to implement the 1588 protocol on a network of 3 hercules MCUs. My knowledge so far gets to the point that the PHY layer is controlled by the DP83640 module on the board for which there is a dedicated enable on the EMAC section of the halcogen settings. Now everything is set up as I see my dedicated source and header file for this module in the CCStudio project. What i would like to know is if there are any examples of the set up of the software to implement the various messages and consequent clock modification that has to be carried out for the network clock synchronyzation. The only functions i can see are aimed to understand what the partner board (?) status is but there nothing in the source file that would enable a possible 1588 message to be sent or received or analyzed.
Thanks in advance for your help
Valentino