Part Number: TMS570LC4357
Hi,
I have a similar question.
The safety goal is DC 90%.
We aim to have external 16M SDRAM.
I agree if there is only data in the external SDRAM, we can use CRC to have an end-to-end protection.
But what if there are instructions running in SDRAM, when there is soft-error in the SDRAM to make some bits of SDRAM incorrect...
Do you have some good advices on how to make DC of that part achieve 90%?