This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS570LC4357: Does the TMS570LC4357 support the nCPUHALTm signal

Part Number: TMS570LC4357
Other Parts Discussed in Thread: SEGGER

The Cortex-R5 core has an input signal "nCPUHALTm"..

This is described in

"http://infocenter.arm.com/help/index.jsp?topic=/com.arm.doc.ddi0460d/BEIBGHGC.html"

If the signal is asserted, then the CPU will not execute any instructions after reset.

  • Is this signal accessible to JTAG probes?
  • Is this documented somewhere?
  • Is this used in the XDS200 driver?

We have IAR I-Jet, Segger J-Link and XDS200 and have seen problems that the CPU
seems to execute code between the reset, and when the CPU is stopped when
we press reset in the IAR GUI.

Best Regards

Ulf Samuelsson

  • Hello,

    Excuse us for the delay in answering. TI Code Composer Studio does support a "Break on Reset" feature for Cortex R4/5 processors. However, I am not sure about the implementation details for this. Hence I am not able to answer whether this feature uses the nCPUHALT input to the CPU or not.

    I am waiting on input from the design team to confirm this and will provide an update as soon as I hear back.

    Regards, Sunil

  • This signal is tied to '1' so that this mechanism is not available for tools to use.