Part Number: TM4C123GH6PM
Hi,
Please help me with some example.
Currently I am using boot_serial Application to download firmware to controller, but when this serial communication breaks while downloading firmware, I need to re-flash boot loader which is problem for me.
I need system stay up if communication during firmware downloading breaks.
I want to Copy the firmware file to flash first as currently my firmware is using only 40% controller flash memory so 60% is free , after complete download i want to run the downloaded firmware if it is valid.
Please suggest some example or correct method.
Thanks,
Pradeep Kumar