Other Parts Discussed in Thread: TM4C129XNCZAD,
Tool/software: Code Composer Studio
I'm trying to start with the USB sample code listed in the header to my bespoke board. In prior questions I posted I was told that this was the recommended way to proceed. So I have a copy of the code in a project created for the TM4C1290NCPDT. In targetConfigs/Tiva TM4C1290NCPDT.ccxml [Active] the processor and the Connection are correct. In usbserialdevice.cfg [TI-RTOS] (in XDCtools) -> Program the Platform Information shows Device name = TM4C129XNCZAD. If I go to Project -> RTSC Tools -> Platform -> Edit/View brings up the "activity spinner" but nothing ever happens and I have to kill CCS.
CCS 8.3.1.00004
XDCtools (I don't know which one is actually being used) 3.30.1.25, 3.51.1.18, 3.31.0.24, 3.32.2.25, 3.32.0.06 and IDE Tooling is 3.51.1.18
tirtos_cc13xx_cc26xx_2_21_00_06
tirtos_tivac_2_16_00_08
Any help on how I should proceed to do this migration would be greatly appreciated.
Thanks
P.S. I've contacted Mindshare Advantage to try to get some consulting help with this but have yet to hear back. Recommendations for any other consultants would also be appreciated.