Part Number: LAUNCHXL2-570LC43
Tool/software: Code Composer Studio
I used HALCoGen to generate software code to communicate 2 LAUNCHXL2-570LC43 MCUs through MIBSPI3, the 2 MCUs transfer and receive an array of 128 word(16-bits), then I configured DMA to write and read data from MIBSPI TX/RX RAM.
At 1MHz, and 2MHz MIBSPI frequency the received data are fine, but at higher MIBSPI frequencies starts from 3MHz!! the received data become corrupted (the elements values are correct but their indices in the array is wrong) each new 128 word received are out of index from the previous reception and so on.
here is the DMA configuration and main function:
#include "SPI_Start.h"
#include "HL_sys_dma.h"
#define D_SIZE 128
#pragma SET_DATA_SECTION(".sharedRAM")
uint16 TXDATA[D_SIZE]; /* transmit buffer in sys ram */
uint16 RXDATA[D_SIZE]= {0}; /* receive buffer in sys ram */
#pragma SET_DATA_SECTION()
#define D_SIZE 128
void mibspiDmaConfig(mibspiBASE_t *mibspi,uint32 channel, uint32 txchannel, uint32 rxchannel)
{
uint32 bufid = D_SIZE - 1;
uint32 icount = 0;
/* setting transmit and receive channels */
mibspi->DMACTRL[channel] |= (((rxchannel<<4)|txchannel) << 16);
/* enabling transmit and receive dma */
mibspi->DMACTRL[channel] |= 0x8000C000;
/* setting Initial Count of DMA transfers and the buffer utilized for DMA transfer */
mibspi->DMACTRL[channel] |= (icount << 8) |(bufid<<24);
}
g_dmaCTRL g_dmaCTRLPKT1, g_dmaCTRLPKT2; /* dma control packet configuration stack */
void main(void)
{
uint8_t i;
for (i=0; i<D_SIZE; i++)
{
TXDATA[i]= i;
}
SPI_Init();
/* - configuring dma control packets */
g_dmaCTRLPKT1.SADD = (uint32)TXDATA; /* source address */
g_dmaCTRLPKT1.DADD = (uint32)&(mibspiRAM3->tx[0].data); /* destination address */
g_dmaCTRLPKT1.CHCTRL = 0; /* channel control */
g_dmaCTRLPKT1.FRCNT = 1; /* frame count */
g_dmaCTRLPKT1.ELCNT = D_SIZE; /* element count */
g_dmaCTRLPKT1.ELDOFFSET = 4; /* element destination offset */
g_dmaCTRLPKT1.ELSOFFSET = 0; /* element destination offset */
g_dmaCTRLPKT1.FRDOFFSET = 0; /* frame destination offset */
g_dmaCTRLPKT1.FRSOFFSET = 0; /* frame destination offset */
g_dmaCTRLPKT1.PORTASGN = PORTA_READ_PORTB_WRITE;
g_dmaCTRLPKT1.RDSIZE = ACCESS_16_BIT; /* read size */
g_dmaCTRLPKT1.WRSIZE = ACCESS_16_BIT; /* write size */
g_dmaCTRLPKT1.TTYPE = FRAME_TRANSFER ; /* transfer type */
g_dmaCTRLPKT1.ADDMODERD = ADDR_INC1; /* address mode read */
g_dmaCTRLPKT1.ADDMODEWR = ADDR_OFFSET; /* address mode write */
g_dmaCTRLPKT1.AUTOINIT = AUTOINIT_ON; /* autoinit */
g_dmaCTRLPKT2.SADD = (uint32)&(mibspiRAM3->rx[0].data); /* source address */
g_dmaCTRLPKT2.DADD = (uint32)RXDATA; /* destination address */
g_dmaCTRLPKT2.CHCTRL = 0; /* channel control */
g_dmaCTRLPKT2.FRCNT = 1; /* frame count */
g_dmaCTRLPKT2.ELCNT = D_SIZE; /* element count */
g_dmaCTRLPKT2.ELDOFFSET = 0; /* element destination offset */
g_dmaCTRLPKT2.ELSOFFSET = 4; /* element destination offset */
g_dmaCTRLPKT2.FRDOFFSET = 0; /* frame destination offset */
g_dmaCTRLPKT2.FRSOFFSET = 0; /* frame destination offset */
g_dmaCTRLPKT2.PORTASGN = PORTB_READ_PORTA_WRITE;
g_dmaCTRLPKT2.RDSIZE = ACCESS_16_BIT; /* read size */
g_dmaCTRLPKT2.WRSIZE = ACCESS_16_BIT; /* write size */
g_dmaCTRLPKT2.TTYPE = FRAME_TRANSFER ; /* transfer type */
g_dmaCTRLPKT2.ADDMODERD = ADDR_OFFSET; /* address mode read */
g_dmaCTRLPKT2.ADDMODEWR = ADDR_INC1; /* address mode write */
g_dmaCTRLPKT2.AUTOINIT = AUTOINIT_ON; /* autoinit */
/* upto 32 control packets are supported. */
/* - setting dma control packets */
dmaSetCtrlPacket(DMA_CH0,g_dmaCTRLPKT1);
dmaSetCtrlPacket(DMA_CH1,g_dmaCTRLPKT2);
/* - setting the dma channel to trigger on h/w request */
dmaSetChEnable(DMA_CH0, DMA_HW);
dmaSetChEnable(DMA_CH1, DMA_HW);
dmaReqAssign(DMA_CH0, DMA_REQ4); //DMA request line 4 -- TX (last col, Table 6-41)
dmaReqAssign(DMA_CH1, DMA_REQ5); //DMA request line 5 -- RX (last col, Table 6-41)
/* - configuring the mibspi dma , channel 2, MibSPI TX Line -2 , MibSPI RX Line - 3 */
/* MibSPI TX Line and MibSPI RX Line are in the parentheses following MibSPI1 */
/* MibSPI3 transfer group 0*/
dmaEnable();
if(SPI_Module[SPI3].MasterSlave!=SLAVE)
{
// Master puts CS to low
mibspiREG3->PC3&= ~(0x00000002U);
}
mibspiTransfer(mibspiREG3, 0);
while (1)
{
if((mibspiREG3->DMACTRL[0]& 0x8000)!=0x8000)
{
if(SPI_Module[SPI3].MasterSlave!=SLAVE)
{
// Master puts CS to high
mibspiREG3->PC3|= (0x00000002U);
}
mibspiDmaConfig(mibspiREG3,0,2,3);
if(SPI_Module[SPI3].MasterSlave!=SLAVE)
{
// Master puts CS to low
mibspiREG3->PC3&= ~(0x00000002U);
}
mibspiTransfer(mibspiREG3, 0);
}
} // End of while loop
} // End of main()