Part Number: EK-TM4C123GXL
Tool/software: TI C/C++ Compiler
I am trying to build an I2C Master interface using PCF8547(I/O Expander Module). When i am build circuit using level converter MH it working fine , Using TS0108E(TI - level converter ) SDA,SCL lines not working .
when i am checking with logic analyzer, Low end side getting data but in hand of High end side not receiving data , so I'm thinking this may be something I may be doing wrong with the use of the Level converter.
Here's the initialization routine:
void initI2C0(void)
{
//This function is for eewiki and is to be updated to handle any port
//enable I2C module
SysCtlPeripheralEnable(SYSCTL_PERIPH_I2C0);
//reset I2C module
SysCtlPeripheralReset(SYSCTL_PERIPH_I2C0);
//enable GPIO peripheral that contains I2C
SysCtlPeripheralEnable(SYSCTL_PERIPH_GPIOB);
// Configure the pin muxing for I2C0 functions on port B2 and B3.
GPIOPinConfigure(GPIO_PB2_I2C0SCL);
GPIOPinConfigure(GPIO_PB3_I2C0SDA);
// Select the I2C function for these pins.
GPIOPinTypeI2CSCL(GPIO_PORTB_BASE, GPIO_PIN_2);
GPIOPinTypeI2C(GPIO_PORTB_BASE, GPIO_PIN_3);
// Enable and initialize the I2C0 master module. Use the system clock for
// the I2C0 module. The last parameter sets the I2C data transfer rate.
// If false the data rate is set to 100kbps and if true the data rate will
// be set to 400kbps.
I2CMasterInitExpClk(I2C0_BASE, SysCtlClockGet(), false);
//clear I2C FIFOs
HWREG(I2C0_BASE + I2C_O_FIFOCTL) = 80008000;
}
I have done things are TSTS0108E,
1.OE lines -HIGH (3.3V)
2.Checked Module is working fine
TM4C123GXL
1. I2C clock frequency reduced .
2.Used external pullup resistors.
Any ideas what I may be doing wrong?
Thanks ;)
Any