Part Number: TM4C129ENCPDT
Other Parts Discussed in Thread: TPS2052B, TM4C1294NCPDT
TM4C129 support,
I have a list of questions about the USB use on the TM4C129. The customer is using the TM4C129x as the USB host. The slave is an RF module connected by USB on a very short cable, 6" or less. The USB cable will be hard wired in their product. Power (5V) is provided to the RF module over the USB.
Questions:
1) Do I need shielding for the cables? If so, how should the shield be terminated?
2) Do I have to be concerned with 45/90 ohm traces if I keep lines from micro/radio module, very short, an inch or less?
3) I see a lot of USB reference and I think this is due to the option for external phy. What are the exact pins of the Tiva that I will require if I need to connect to the radio module that is in slave mode or OTG? VBUS, D+, D-, Ground?
4) Can I connect them both together in a OTG mode and if so, is there any benefit to doing it that way?
5) USB interface will always be connected so is there still a need for USB detection and VBUS?
6) If VBUS is required, what is the minimum circuit I need to make this work. I have limited space and really did not want to add a 5V switcher as 5V is not present in my design. I only have 12V, 3.3, and 4V. Since there will be 5V being supplied to anything but VBUS, can I get away with a something really simple off the 12V rail like resistor and zener?
7) Do I require an external 5V power supply at all since we are not powering any external devices?
Thanks,
Darren