This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS570LC4357: Tracking HALCoGen errata between 4.07.00 and 4.07.01

Expert 1226 points

Part Number: TMS570LC4357
Other Parts Discussed in Thread: HALCOGEN

We're updating a product that was released with code generated from HALCoGen v4.07.00 to use code generated from HALCoGen v4.07.01.

Our release process includes review and analysis of all known issues with third-party tools and code used to generate our firmware.

v4.07.00 used a format such as "SDOCM00084753" for its errata references, while v4.07.01 uses a format such as "HERCULES_SW-5082".  It is not clear to us in all cases how to map between these references.

Can you please help us align these references properly so that our errata tracking / analysis is correct?

Here is where we are currently at:

v4.07.00 References New-format References Status in v4.07.01 Description
SDOCM00084753 SYS: Since the PLL tab does not spit out warnings if any final or intermediate frequencies generated are out of spec.
SDOCM00086009 Tool: No KEIL tool support for TMS470M devices
SDOCM00087899 FEE: The FEE driver GUI in TMS470Mx family only supports 10 blocks.
SDOCM00095488 CAN: Support for Mixed mode in can driver is necessary.
SDOCM00088096 ADC: interrupt Enable check box for Event, Group1 and Group2 groups for ADC1, ADC2 in HCG.
SDOCM00122504 FEE: HALCoGen FEE Driver Does Not Set Bank Before Writing To Flash.
SDOCM00122496 FEE: HALCoGen FEE Corruption - Block Header Not Written Properly.
SDOCM00122164 SYS: HALCoGen RAM and Stack Locations are Hard-coded.
SDOCM00121738 FEE: FEE Driver Does not Check CRC when reading and crc option is enabled.
SDOCM00122382 SYS: Clock Tree tab to RM57 and TMS570LC43 are not available.

--thx