Other Parts Discussed in Thread: ADS8688, ADS8678, ADS8668, ADS8688A, ADS8698
Hi. I have one of your evaluation boards, specifically ADS86xx EVM. I have tried to install the accompanying GUI from the board on 2 different laptops but I am unable to do so. During the installation process, I get the following 2 errors:
"NI LabVIEW Run-Time Engine 2010 SP1:
Error 1335. The cabinet file ‘lvrte.cab’ required for this installation is corrupt and cannot be used. This could indicate a network error, an error reading from the CD-ROM, or a problem with this package."
"NI Measurement Studio ComponentWorks 3D Graph:
The cabinet file ‘MStudioCW3DGraph.cab’ required for this installation is corrupt and cannot be used. This could indicate a network error, an error reading from the CD-ROM, or a problem with this package."
When I click ignore, the installation process continues but ultimately fails. When I then try to open the GUI using the icon on my desktop, I get the following error:
"Unable to locate the LabVIEW Run-Time Engine:
ADS86XX EVM GUI requires a version 2010 (or compatible) LabVIEW Run-Time Engine. Please contact the vendor of ADS86XX EVM GUI to correct this problem."
Thanks.