Because of the Thanksgiving holiday in the U.S., TI E2E™ design support forum responses may be delayed the week of November 23.

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

RE: TM4C1290NCPDT: assigning interrupt sub group priorties

Guru 56418 points

In response to: https://e2e.ti.com/support/microcontrollers/other/f/908/t/874371

Bob Crosby said:
Here is a table from page 171 of the datasheet that shows the tradeoff between group priorities and sub-priorities:

Yet Tivaware states groups 3-7 have the same effect as group 0-2 and seems to counter table 3-9 being true. The table makes sense but IntPriorityGroupSet() makes the exact opposite argument to table 3-9. Who's on first? 

//*****************************************************************************
//
//! Sets the priority grouping of the interrupt controller.
//!
//! \param ui32Bits specifies the number of bits of preemptable priority.
//!
//! This function specifies the split between preemptable priority levels and
//! sub-priority levels in the interrupt priority specification.  The range of
//! the grouping values are dependent upon the hardware implementation; on
//! the Tiva C and E Series family, three bits are available for hardware
//! interrupt prioritization and therefore priority grouping values of three
//! through seven have the same effect.
//!
//! \b Example: Set the priority grouping for the interrupt controller.
//!
//! \verbatim
//! //
//! // Set the priority grouping for the interrupt controller to 3 bits.
//! //
//! IntPriorityGroupingSet(2);
//!
//! \endverbatim

 

  • Gl said:
    Yet Tivaware states groups 3-7 have the same effect as group 0-2

    Are you referring to the following comment?

    Gl said:
    three bits are available for hardware interrupt prioritization and therefore priority grouping values of three through seven have the same effect

     

    The second statement is not talking about group numbers, rather the value passed to the function IntPriorityGroupinSet(). That value determines how many of the priority bits are used for preemptable groups. Since only three bits are implemented, specifying a value greater than three still only gives you three bits for determining the preemptable groups.  

  • Bob Crosby said:
    The second statement is not talking about group numbers, rather the value passed to the function IntPriorityGroupinSet().

    So the datasheet table group numbers 0x0 - 0x4 don't match the Tivaware function call as to confuse everyone? That older grouping order may be left over from Stellarisware migration since those groups don't match the newer TM4C table.  

    Bob Crosby said:
    greater than three still only gives you three bits for determining the preemptable groups.

    Yet when I tried to set IntPriorityGroupingSet(2) for the same 8 sub priority groups with 23 interrupts it caused odd failures. However IntPriorityGorupingSet(4) works without any issues for several interrupts inside sub priority groups 0x0, 0x20, 0x40, 0x60, 0x80, 0xE0. If group 0-2 had the same effect noting would cause interrupt issues but it does. 

    Bob Crosby said:
    three bits are available for hardware interrupt prioritization and therefore priority grouping values of three through seven have the same effect

    Why does 3-7 exist in the table if those groups can not be split into sub priorities and confuse us the entire table is valid when Tivaware function note claims otherwise. Oddly grouping 4 works and grouping 2 seems like it don't work at all. Also Tivaware example applications have priority grouping 4 configured, why not 0 or 2.

  • Oddly interrupt.c  PRIGROUP_4_4 is 0x300 selects 3 bits for the group priority field (bxxx.) Table 3-9 field bits (0x0 - 0x4) = 8 priority groups 1 sub priority. Perhaps why IntPrioritryGroupingSet(2) selects 0x500 (bxx.y) PRIGROUP 2_6 or 4 groups with 2 sub priorities. It seems the constant names are not exactly split as table 3-9 shows and expected for the TM4C.

    //*****************************************************************************
    //
    // This is a mapping between priority grouping encodings and the number of
    // preemption priority bits.
    //
    //*****************************************************************************
    static const uint32_t g_pui32Priority[] =
    {
        NVIC_APINT_PRIGROUP_0_8, NVIC_APINT_PRIGROUP_1_7, NVIC_APINT_PRIGROUP_2_6,
        NVIC_APINT_PRIGROUP_3_5, NVIC_APINT_PRIGROUP_4_4, NVIC_APINT_PRIGROUP_5_3,
        NVIC_APINT_PRIGROUP_6_2, NVIC_APINT_PRIGROUP_7_1
    };

  • You are confusing "Bit field" with group number. They are not the same. 

    Gl said:
    Yet when I tried to set IntPriorityGroupingSet(2) for the same 8 sub priority groups with 23 interrupts it caused odd failures.

    IntPriorityGroupingSet(2) allocates two bits for preemptable groups (making four preemptable groups) and leaves one bit for sub priority (making two sub-priorities for each group). If you thought that it would give you 8 sub-priority groups, that may be why you got odd failures.

    Gl said:
    IntPriorityGorupingSet(4) works without any issues for several interrupts inside sub priority groups 0x0, 0x20, 0x40, 0x60, 0x80, 0xE0. If group 0-2 had the same effect noting would cause interrupt issues but it does. 

    IntPriorityGroupingSet(4) will allocate all 3 bits to preemptable groups. It is exactly the same as IntPriorityGroupingSet(3). Here is the table in another form to help make it more clear:

    IntPriorityGroupingSet(0)  no bits for premeptable groups, 8 sub-priority groups

    IntPriorityGroupingSet(1)  one bit for premeptable groups, two preemptable groups each having 4 sub-priority groups

    IntPriorityGroupingSet(2)  two bits for premeptable groups, four preemptable groups each having two sub-priority groups

    IntPriorityGroupingSet(3)  three bits for premeptable groups, eight preemptable groups, no sub-priority groups

    IntPriorityGroupingSet(4)  three bits for premeptable groups, eight preemptable groups, no sub-priority groups

    IntPriorityGroupingSet(5)  three bits for premeptable groups, eight preemptable groups, no sub-priority groups

    IntPriorityGroupingSet(6)  three bits for premeptable groups, eight preemptable groups, no sub-priority groups

    IntPriorityGroupingSet(7)  three bits for premeptable groups, eight preemptable groups, no sub-priority groups

  • Gl said:
    It seems the constant names are not exactly split as table 3-9 shows and expected for the TM4C.

    Those defines are used to create a constant table used by the IntPriorityGroupingSet() function. The meaning of the names is the number of bits for group priority as opposed to sub-priority. The confusion comes because the table is created for the maximum possible bits, 8, but the TM4C only implements 3. 

    The TivaWare driver function IntPriorityGroupingSet() was designed to simplify setting the number of preemptable groups and sub-priority groups. The NVIC_APINT_PRIGROUP_x_y constants are for internal use of the function and are not to be used as arguments to the function.

  • Bob Crosby said:
    IntPriorityGroupingSet(4) will allocate all 3 bits to preemptable groups. It is exactly the same as IntPriorityGroupingSet(3). Here is the table in another form to help make it more clear:

    So datasheet table 3-9 is not telling the truth of how priority groups and sub priority must exist in row 1 last 2 columns.

    I read table 3-9 row 1 as 0x0 - 0x4 all produce 8 group priorities 1 sub priority in each group. So 0x0-0x4 results in the same grouping according row 1 last 2 columns. It would be improper to make a table outcome of only one selections, 0x0 - 0x4. Doing such would invalidate all the other configurations and make the table less than informational, more confusing to the reader. 

    However priority group field 1st column (0x5, 0x6, 0x7) will result in the specific grouping, sub order shown in the last 2 columns. Tivaware sets the PRIGROUP bit field [10:8] APINT register as show below table 3-9, relative to 1st column. Table 3-9 is talking about APINT bits [10:8] not Tivaware contsants used to configure APINT register bits. The constants for APINT have 0x000 - 0x004, 0x500, 0x600, 0x700 in the same [10:8] bits shown in table 3-9.  

    Bob Crosby said:
    IntPriorityGroupingSet(2)  two bits for premeptable groups, four preemptable groups each having two sub-priority groups

     

    That sort of blows a hole in table 3-9 lay out and most will easily forget that several months from now.

  • Bob Crosby said:
    The confusion comes because the table is created for the maximum possible bits, 8, but the TM4C only implements 3. 

    So table 3-9 is not for TM4C1294 MCU and some other MCU?

    Has table 3-9 been corrected in a later datasheet versions as readers with short term memory loss may forget this thread ever existed 6 months from now?

  • Forgot new Acrobat reader has built add of sticky notes into unlocked PDF. So added above new table 3-9 group definitions to the datasheet as a bug note.

  • Table 3-9 is correct, but column one is the bitfield of the APINT register, not the parameter that is passed to the IntPriorityGroupingSet() function. 

    IntPriorityGroupingSet(7) will result in 0 being programmed into the three bits of PRIGROUP bit field and will result in 8 groups each with a single sub-priority group.

    IntPriorityGroupingSet(6) will result in 1 being programmed into the three bits of PRIGROUP bit field and will result in 8 groups each with a single sub-priority group.

    IntPriorityGroupingSet(5) will result in 2 being programmed into the three bits of PRIGROUP bit field and will result in 8 groups each with a single sub-priority group.

    IntPriorityGroupingSet(4) will result in 3 being programmed into the three bits of PRIGROUP bit field and will result in 8 groups each with a single sub-priority group.

    IntPriorityGroupingSet(3) will result in 4 being programmed into the three bits of PRIGROUP bit field and will result in 8 groups each with a single sub-priority group.

    IntPriorityGroupingSet(2) will result in 5 being programmed into the three bits of PRIGROUP bit field and will result in four groups each with two sub-priority groups.

    IntPriorityGroupingSet(1) will result in 6 being programmed into the three bits of PRIGROUP bit field and will result in two groups each with 4 sub-priority groups.

    IntPriorityGroupingSet(0) will result in 7 being programmed into the three bits of PRIGROUP bit field and will result in one group with 8 sub-priority groups.

  • Bob Crosby said:
    Table 3-9 is correct, but column one is the bitfield of the APINT register, not the parameter that is passed to the IntPriorityGroupingSet() function.

    Check again as it shows below address offset and is the hex/binary code for bits [10:8]

    Application Interrupt and Reset Control (APINT)

    Base 0xE000.E000
    Offset 0xD0C
    Type RW, reset 0xFA05.0000

  • That is correct. Coming out of reset you have 8 groups each with a single sub-priority group.

  • There is always the distinct possibility table 3-9 is correct and the NVIC is acting more like you have outlined in your above table listing. Perhaps edit 0x0 above to indicate 1 sub priority. Interrupt/s having the lowest number with in the sub priority in each group have priority over higher number interrupts. That is how 23 interrupts can allow NVIC tail chaining to work so well, keeping that in mind.

  • Bob Crosby said:
    Coming out of reset you have 8 groups each with a single sub-priority group.

    Decided to test grouping 0x0 after you mention above for the same 23 interrupts 8 groups. What happened next was odd sequential phasing between all the interrupts occurred. It seems 0x3-0x4 are 8 groups 1 sub priority being the interrupt number value within each group.