This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CCS/TM4C123GH6PM: Confused about Clock Frequency in flash settings in debug in CCS

Part Number: TM4C123GH6PM

Tool/software: Code Composer Studio

Hi,

When you go to project properties - debug - flash settings, the crystal frequency setting there, is that referring to the system clock or the external crystal frequency? In the case of the TM4C123 launchpad, I''ve set the system clock to 80MHz. Should I enter 80MHz in the blank or should it be 16MHz? I tried both and I did not notice anything happen. Please clarify this.

Thanks.

Regards,

AJ