This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS570LC4357: MEMORY

Part Number: TMS570LC4357

Hi. I am thinking of operating with the following configuration. GCLK:300MHz, HCLK:150MHz, RWIT:3 Q1:If the cache is used, can the flash memory and SRAM access speed be considered 300 MHz? Q2:If the cache is not used, can the flash memory and SRAM access speed be considered as 150MHz? Best Regards.