Other Parts Discussed in Thread: UNIFLASH
We have encountered some issues with our LM3S9B92-IQC80-C5 design. The Product has been in service for about 5 years now, and we are seeing an increasing number with the same CPU failure.
The CPU will not boot up on Power-On, our observations is:
- 3.3V VDD power is ok.
- Power consumption is normal.
- VDD voltage is ok (1.30 V)
- Main Crystal pin 49 is High (no oscillation)
- PHY Crystal pin 17 is High (no oscillation)
- Bootloader (serial) does not work (with LM Flash programmer)
- Cannot be programmed from Debug probe (XDS100v2)
We know the CPU is obsolete.
Any ideas what could cause this?
Best Regards
Henning Christinansen