This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS570LC4357, example spna217.pdf, two sine waves in one HET



Hi all,

I want to generate two different PWMs (sine waves with different amplitude and frequency) but from one HET time Processor on my eval board TMS570LC43x HDK.

So I just used the example spna217.pdf and this is already running.

My idea is to copy the actual HET source Code and use it for a second PWM signal with register B, like this:


PWM_PERIOD            .equ 1
PWM_PIN_NUM4          .equ 4
PWM_PIN_NUM2          .equ 2
INIT_COMPARE          .equ 1
INIT_HR_DELAY         .equ 0


L00   CNT { reqnum=0,request=GENREQ,reg=A,irq=OFF,max=1};
L01   ECMP { next=L03,hr_lr=HIGH,en_pin_action=ON,cond_addr=L02,pin=PWM_PIN_NUM2, action=PULSELO,reg=A,irq=OFF,data=INIT_COMPARE,hr_data=INIT_HR_DELAY};
L02   MOV32 { remote=L01,type=IMTOREG&REM,reg=A,data=INIT_COMPARE,hr_data=INIT_HR_DELAY};


L03   CNT { reqnum=0,request=GENREQ,reg=B,irq=OFF,max=1};
L04   ECMP { next=L06,hr_lr=HIGH,en_pin_action=ON,cond_addr=L05,pin=PWM_PIN_NUM4, action=PULSELO,reg=B,irq=OFF,data=INIT_COMPARE,hr_data=INIT_HR_DELAY};
L05   MOV32 { remote=L04,type=IMTOREG&REM,reg=B,data=INIT_COMPARE,hr_data=INIT_HR_DELAY};

L06   BR { next= L00, cond_addr=L00, event= NOCOND }


so the next step was to set up the HTU like this. I think I can use the register IFADDRB for the second PWM Signal.

void htuInit(void){
    /* DCP0 CPx element count = 1, frame count = SAMPLE_SIZE */
    htuDCP1->ITCOUNT = 0x00010000 + SAMPLE_SIZE;
    /* DCP0 CPx DIR = main memory to NHET */
    /* SIZE = 32-bit */
    /* ADDMH = 16 bytes */
    /* ADDFM = post-increment main memory */
    /* TMBA = circular buffer A */
    /* TMBB = one shot buffer B (buffer B not used) */
    /* IHADDR = 0x28 MOV32 data field */
    htuDCP1->IHADDRCT = (htuDCP1->IHADDRCT & 0x0) |
    0x1 << 23 | // DIR
    0x0 << 22 | // SIZE
    0x0 << 21 | // ADDMH
    0x0 << 20 | // ADDFM
    0x1 << 18 | // TMBA
    0x0 << 16 | // TMBB
    0x28 << 0; // IHADDR
    /* DCP0 CPA start address of source buffer */
    htuDCP1->IFADDRA = (unsigned int)sine_table;
    htuDCP1->IFADDRB = (unsigned int)sine_table2;
    /* enable DCP0 CPA */
    htuREG1->CPENA = 0x00000001;
    /* enable HTU */
    htuREG1->GC = 0x00010000;
}


and also my configNHET1 function like this:

void configNHET1(void)
{
    hetREG1->PFR = LRPFC << 8;
    calculate_ecmp_compare();

    hetREG1->REQENS = 1 ;

    hetREG1->DIR |= (1 << PIN_HET_2) ;
    hetREG1->DIR |= (1 << PIN_HET_4) ;

    hetRAM1->Instruction[pHET_L00_0].Control  = (hetRAM1->Instruction[pHET_L00_0].Control & 0xFFFD0000) | (uint32)(CNT_MAX_PERIOD - 1);
    hetRAM1->Instruction[pHET_L03_0].Control  = (hetRAM1->Instruction[pHET_L03_0].Control & 0xFFFD0000) | (uint32)(CNT_MAX_PERIOD - 1);

    hetRAM1->Instruction[pHET_L01_0].Control  = (hetRAM1->Instruction[pHET_L01_0].Control & 0xFFFFE0FF) | (PIN_HET_2 << 8);
    hetRAM1->Instruction[pHET_L04_0].Control  = (hetRAM1->Instruction[pHET_L04_0].Control & 0xFFFFE0FF) | (PIN_HET_4 << 8);
}

The first PWM is running, but I have  problems with the second one. I get a PWM Signal with a fixed duty cycle on the second channel.

Best regards

Lars

 

  • Hi Lars,

    I will take a look at your question later, and come back to you as soon as I can. 

  • Hi Lars,

    Please use DCP[0] for teh 1st PWM, and use DCP[1] for the 2nd PWM.

    htuRAM1 ->DCP[0].IFADDRA = (unsigned int)sine_table2;

  • Hi all,

    I think that will work, I am sure. But than I used the second HTU.

    But I need the second HTU plus second HET Processor for other thinks, like a triangle signal.

    So what I want is to do is to generate two sine waves with different frequencies and amplitude with one HET and one HTU.

    Best regards

    Lars

  • Hi Lars,

    I didn't mean to use N2HET2 and HTU2. I mean to use HTU1 control packet 0 (DCP[0]) for sine_table1 and use HTU1 control packet 1 (DCP[1]) for sine_table2.

  • Hi all,

    I adapt my files HL_reg_htu.h and configHtu.c as followed. Now I hopefully use DCP[0] and DCP[1]. The Register IFADDRA, IHADDRCT, ITCOUNT are now initialized for DCP[0] and DCP[1], I also set the CPENA Register to 0x05u.

    But I got the same result. First PWM is running, the second one is still a PWM Signal with a fixed duty cycle..


    HL_reg_htu.h:

    /* USER CODE BEGIN (1) */

    typedef volatile struct dcp
    {
        htudcp_t dcp[8];
    } dcp_t;

    #define htuRAM1   ((dcp_t *)0xFF4E0000U)
    /* USER CODE END */


    configHtu.c:

    void htuInit(void){
        /* DCP0 CPx element count = 1, frame count = SAMPLE_SIZE */
    //    htuDCP1->ITCOUNT = 0x00010000 + SAMPLE_SIZE;
        htuRAM1->dcp[0].ITCOUNT = 0x00010000 + SAMPLE_SIZE;
        htuRAM1->dcp[1].ITCOUNT = 0x00010000 + SAMPLE_SIZE;
        /* DCP0 CPx DIR = main memory to NHET */
        /* SIZE = 32-bit */
        /* ADDMH = 16 bytes */
        /* ADDFM = post-increment main memory */
        /* TMBA = circular buffer A */
        /* TMBB = one shot buffer B (buffer B not used) */
        /* IHADDR = 0x28 MOV32 data field */
    #if(0)
        htuDCP1->IHADDRCT = (htuDCP1->IHADDRCT & 0x0) |
        0x1 << 23 | // DIR
        0x0 << 22 | // SIZE
        0x0 << 21 | // ADDMH
        0x0 << 20 | // ADDFM
        0x1 << 18 | // TMBA
        0x0 << 16 | // TMBB
        0x28 << 0; // IHADDR
    #else
        htuRAM1->dcp[0].IHADDRCT = (htuRAM1->dcp[0].IHADDRCT & 0x0) |
        0x1 << 23 | // DIR
        0x0 << 22 | // SIZE
        0x0 << 21 | // ADDMH
        0x0 << 20 | // ADDFM
        0x1 << 18 | // TMBA
        0x0 << 16 | // TMBB
        0x28 << 0; // IHADDR

        htuRAM1->dcp[1].IHADDRCT = (htuRAM1->dcp[1].IHADDRCT & 0x0) |
        0x1 << 23 | // DIR
        0x0 << 22 | // SIZE
        0x0 << 21 | // ADDMH
        0x0 << 20 | // ADDFM
        0x1 << 18 | // TMBA
        0x0 << 16 | // TMBB
        0x28 << 0; // IHADDR
    #endif
        /* DCP0 CPA start address of source buffer */
    //    htuDCP1->IFADDRA = (unsigned int)sine_table;
    //    htuDCP1->IFADDRB = (unsigned int)sine_table2;
        htuRAM1->dcp[0].IFADDRA = (unsigned int)sine_table;
        htuRAM1->dcp[1].IFADDRA = (unsigned int)sine_table2;
        /* enable DCP0 CPA */
    //    htuREG1->CPENA = 0x00000001;
        htuREG1->CPENA = 0x00000005;
        /* enable HTU */
        htuREG1->GC = 0x00010000;
    }

    Best regards

    Lars

  • Hi all,

    I also do the following changes:

    old code

    hetREG1->REQENS = 1;

    new code

    hetREG1->REQENS = 2;

    and set reqnum to 1

    L03   CNT { reqnum=1,request=GENREQ,reg=B,irq=OFF,max=1};

    May be it is better if I post the complete project.

    Best regards

    Lars6431.PWM.ZIP

  • Hi all,

    I found my SW bug. The data for the register htuRAM1->dcp[1].IHADDRCT were wrong.

    The second DMA reguest is at Code line 4 in file file sinus.het. So I must set the IHADDR = 0x58.

    Thanks a lot, best regards

    Lars