Tool/software: Code Composer Studio
Hi,
i am working with sensor Boost that contain MPU-9150 sensor using TivaC123 sensor algorithm from Ti and when debugging the code on board changing in the system frequency or the delay between write configuration and read using I2C from the sensor, i found that the readings changes but also give me wrong readings when comparing it with the mobile application readings for gyroscope, accelerator, and magnetometer.
i need to know the right value of function delay that i need to set to get the accurate readings while using the maximum frequency from the internal oscillator of the master MCU.