Because of the Thanksgiving holiday in the U.S., TI E2E™ design support forum responses may be delayed the week of November 23.

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Compiler/RM48L952: Running tcp/ip stack + freertos on RM48L952ZWT

Part Number: RM48L952
Other Parts Discussed in Thread: HALCOGEN

Tool/software: TI C/C++ Compiler

Hello Team,

I have successfully ran freertos on my hercules micro-controller RM48L952ZWT. Also, I successfully implemented LWIP stack on the micro- controller.

The code is generated through HALCOGEN. I have done both the tasks separately and now when I tried to generate a code for Freertos plus LWIP together through halcogen, I was successful in getting my build through.

But, during testing of the device I am not able to run both together. Only one can run at a time.

I am not sure how to run both the things at once.

For developing freertos I used:-

https://www.ti.com/lit/an/spna237/spna237.pdf

For developing Lwip I used

http://www.ti.com/lit/an/spna239/spna239.pdf

Please let me know what amendments I need to make.

My guess is I need to make some changes in my linker file to adjust the memory.

Below is main.c file

#include "sys_common.h"

#include "system.h"

#include <stdio.h>

#include "gio.h"

#include "emac.h"

/* USER CODE BEGIN (1) */

/* USER CODE BEGIN (1) */

/* Include FreeRTOS scheduler files */

#include "FreeRTOS.h"

#include "os_task.h"

/* USER CODE END */

/* Include HET header file - types, definitions and function declarations for system driver */

#include "het.h"

#include "gio.h"

/* Define Task Handles */

xTaskHandle xTask1Handle_1;

xTaskHandle xTask1Handle_2;

xTaskHandle xTask1Handle_3;

uint8    emacAddress[6U] =   {0x00U, 0x08U, 0xEEU, 0x03U, 0xA6U, 0x6CU};

uint32  emacPhyAddress  =   1U;

extern void EMAC_LwIP_Main (uint8_t * emacAddress);

/* Task1 */

void vTask1(void *pvParameters)

{

    for(;;)

    {

        /* Taggle HET[1] with timer tick */

        gioSetBit(hetPORT1, 16, gioGetBit(hetPORT1, 16) ^ 1);

       vTaskDelay(1000);

    }

}

/* Task2 */

void vTask2(void *pvParameters)

{

   int count1 = 0;

   for(;;)

   {

        /* Taggle HET[1] with timer tick */

    gioSetBit(hetPORT1, 27, gioGetBit(hetPORT1, 27) ^ 1);

     count1++;

     vTaskDelay(1000);

      if(count1 == 8)

       vTaskDelete(xTask1Handle_2);

   }

}

void vTask3(void *pvParameters)

{

   int count2 = 0;

   while(1)

   {

        /* Taggle HET[1] with timer tick */

        gioSetBit(hetPORT1, 05, gioGetBit(hetPORT1, 05) ^ 1);

        count2++;

       vTaskDelay(1000);// 1 sec delay

        if(count2 == 8)

        vTaskDelete(xTask1Handle_3);

   }

}

/** @fn void main(void)

*   @brief Application main function

*   @note This function is empty by default.

*

*   This function is called after startup.

*   The user can use this function to implement the application.

*/

/* USER CODE BEGIN (2) */

/* USER CODE END */

int main(void)

{

/* USER CODE BEGIN (3) */

    gioInit();

    EMAC_LwIP_Main(emacAddress);

    /* Set high end timer GIO port hetPort pin direction to all output */

        gioSetDirection(hetPORT1, 0xFFFFFFFF);

        /* Create Task 1 */

              if (xTaskCreate(vTask1,"Task1", configMINIMAL_STACK_SIZE, NULL, 1, &xTask1Handle_1) != pdTRUE)

               {

                   /* Task could not be created */

                 while(1);

               }

               /* Create Task 1 */

            if (xTaskCreate(vTask2,"Task2", configMINIMAL_STACK_SIZE, NULL, 1, &xTask1Handle_2) != pdTRUE)

            {

                 /* Task could not be created */

              while(1);

            }

            if (xTaskCreate(vTask3,"Task3", configMINIMAL_STACK_SIZE, NULL, 1, &xTask1Handle_3) != pdTRUE)

                  {

                     /* Task could not be created */

                    while(1);

                 }

               /* Start Scheduler */

                vTaskStartScheduler();

               /* Run forever */

              while(1);

 /* USER CODE END */

}