Other Parts Discussed in Thread: HALCOGEN
Hi,
I hope someone could help to explain some points,
According to the http://e2e.ti.com/support/microcontrollers/tms570/f/312/p/57753/205375.aspx#205375
to setup the FreeRTOS in TMS570 the '_svc' should replace with 'vPortYieldProcessor'.
I have seen in the TMS Safety Demos there is one file "sys_svc.asm" that is used to enable and disable FIQ and IRQ
1. Should be this implemented for the FreeRTOS too?
2. What happens to the interrupts during STC/LBIST tests is Running?
3. I Have used "xTaskCreate" to create a task and inside it started the STC test for the cores, but it hang-up.. dont now why.
Have i missed something that i should take care?
4. How interacts/are linked the ISR with the FreeRTOS isr?
Regards Burim