Part Number: TMS570LC4357
Other Parts Discussed in Thread: TMS570LS3137, , HALCOGEN
Hello,
I'm using TMS570LC43 HDK board with our software that I ported from TMS570LS3137 and I am getting some ESM error when I power up:
1. ESM Group1 bit 47 - ACP d-cache invalid.
2. ESM Group 1 bit 52 - CPU Interconnect Subsystem-Global Error appears sometimes after power up (intermittent).
3. After I connect with the emulator (XDS560V2 STM USB), I get ESM Group 1 bit31 and Group 2 bit 2 (CCM-R5F - self-test and CCM-R5F - CPU Compare error. I do not reset the processor on connect, however the error pops up on connection. I transmit the ESM status registers on CAN and monitor it and I see errors (1) and (2), but not this one, so I know that it is on connect, as I see it on the ESM registers on the debugger.
After those errors are cleared in ESM High Interrupt routine, the code keeps running with no errors.
Any suggestions why I get those errors and how can I avoid them?
Thanks,
Alex