Because of the Thanksgiving holiday in the U.S., TI E2E™ design support forum responses may be delayed the week of November 23.

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS570LS3137: UNIFLASH fails flashing application with embedded ECC

Part Number: TMS570LS3137
Other Parts Discussed in Thread: UNIFLASH, TMS570LC4357,

Dear all, I writing you in order to get your help in understand what's wrong in my procedure.

How can I get over the issue?

Thanks, Best regards

Silvano Battisti

ISSUE: uniflash 5.3 (but all versions) fails flashing an application that includes the ECC generated by linker command.

I try to download an application that includes the flash ECC ( NO uniflash auto_ECC).

The download fails in verifying the ECC (at address 0xf0400000)

What's wrong?

Steps to produce the issue

  • Erase chip
  • PowerOff
  • PowerOn
  • Load program

See attached zipped project4118.TestUniflash_R00.zip

  • Hello Silbvano,

    If using linker cmd to generate ECC, when loading the code to flash:

    1. Auto ECC Generation Must be unchecked
    2. Perform Blank Check before Program Load Must be unchecked
    3. Flash Verification Settings Must be 'None'

    The flash bank width is 144 bits wide including 128 data bits and 16 ECC bits. In either standard read mode or pipeline read mode, 128 bits data and 16 bits ECC is read at a time.

    If "AUTO ECC Generation" is enabled, the CCS loader will generate 16-bit ECC for every 128-bit data, and program those 144 bits data to flash at a time.

    If using Linker to generate ECC, the ECC data is generated using obj files at link stage and ECC data is placed in out file. When loading data, the loader will program the whole data section first, then ECC section. If the data verification is enabled, the written data (plus 16 bits ECC) will be read back every 128-bit write-operation for verification, but the ECC data has not programmed at this moment. So the ECC error will be generated, and the error pin will set too.

  • Dear Wang,

    thanks for your replay.

    Using the suggested settings, the download runs, but after that a the "Verify Image" fails. It seams that the ECC section hasn't been correctly programmed anyway.

    Uniflash logs:
    [28/2/2020 08:17:52] [INFO] CortexR4: GEL Output: Memory Map Setup for Flash @ Address 0x0 due to System Reset
    [28/2/2020 08:17:54] [SUCCESS] Program Load completed successfully.
    [28/2/2020 08:17:57] [INFO] CortexR4: GEL Output: Memory Map Setup for Flash @ Address 0x0
    [28/2/2020 08:18:12] [ERROR] CortexR4: File Loader: Verification failed: Values at address 0xF0400000 do not match Please verify target memory and memory map.
    How can I get over?
    Thanks
    Best Regards
    Silvano

      

  • Hello Silvano,

    As I said in my last post, please don't so file verification. 

  • Hallo Wang,

    Yes of course I did. My procedure was:

    1) Erase the Flash   -> SUCCESS

    2) target power off /power on

    3) Load image without any verification  ("no" blank check,  "none" verification)    ->SUCCESS

    4) target power off /power on

    5) Verify Image -> ERROR

    So my question is: removing above steps 4 and 5,  how can I get evidence that what is chip flash is what I have in program file?

    Thank you very much

    Best Regards

    Silvano Battisti

  • Hello,

    Checked your linker cmd file. You don't map .intvecs to VECTORS in SECTIONS of your linker cmd file. 

    I did a test of verifying a image (ECC generated throught linker cmd) on uniflash, and it works well:

  • Dear Wang,

    Thank you for your reply. I really appreciate your feedback. I'm so sorry for bothering you.

    Yes you are in right the vector wasn't included. It is a very dummy project. I wasn't really interested in a running project but something to download instead of my final application (that has the same flashing issue).  

    Anyway, I've added the missing in link command file. But the result doesn't change: failure.

    I see your test on the TMS570LC43 family works. Is it a dummy test project? If it is a dummy project could you post it to me so I can try adapting to my TMS family? How written above, I'm not really interested in a running project but in something to flash by JTAG using Uniflash.

    My concern is about something missing or wrong in the download session configuration for Uniflash.

    Thank you very much again for your support.

    Best Regards

    Silvano Battisti

    PS: I've attached the last test project4186.TestUniflash_R02.zip

  • You can find the project used for my test (TMS570LC4357 CAN bootloader):

    https://git.ti.com/hercules_examples

  • Dear Wang,

    thanks for your example projects.

    I build the ls31_can_boot application. I have got the issue.  Moreover I try a build of lc43_can_boot application (after resizing the flash in command link file). I've got the issue again.

    Notice that the failure happen on a "virgin" device. You must erase the flash of the micro, power off, power on and than load the application. When you download the application again (on a programmed device) the issue doesn't trigger.

    Step to have the issue:

    1) Erase the flash  -> SUCCESS

    2) Power off

    3) Power on

    4) Load Application without any verification -> SUCCESS

    5) Verify Application -> FAILURE

    6) Load Application without any verification -> SUCCESS

    7) Verify Application -> SUCCESS

    Remark that my CPU is a TMS570LS3137

    Can you help me understanding what is happen?

    Thank you very much

    Best Regards

    Silvano Battisti

  • Hello,

    Can you please dump the memory content at 0xF0400E9A and 0x000074D0 (LC4357 device) and 0xF0401358 and 0x00009AC0 (LS3137) of failed and successful verification?

    I tested on LC43x launchpad, but I don't have board for LS3137. 

  • Dear Wang,

    Thank you very much for your support

    Best Regards

    Silvano Battisti

    Look at the attached files:

    LC43.zip includes the ELF program, the whole dump of ECC bank 0  in failure the dump of whole ECC bank 0 in success and the dump of program limited at 0x10000 bytes.

    LS31.zip includes the ELF program, the whole dump of ECC bank 0  in failure the dump of whole ECC bank 0 in success and the dump of program limited at 0x10000 bytes.

    Here the difference in ECC at verification failure address 0xF0400E9A including corresponding program flash address.
      -> ECC origin offset 0xE9A
      -> Corresponding program offset = 0xE9A * 8 = 0x74D0

    It appears that at "virgin" programming, the ECC stops to be written at the end of the programming address.   I.E. the uniflash stops programming ECC for the bank 0 "filled" region.

    Here the difference in ECC at verification failure address 0xF040135B including corresponding program flash address.
      -> ECC origin offset 0x135B
      -> Corresponding program offset = 0x135B * 8 = 0x9AD8

    Same as above.

    3252.lc43.zip

    2772.ls31.zip

  • Hello,

    It looks like that the fill portion is not programmed. Do you see the same issue with CCS? 

  • Dear Wang,

    Yes it is. The fill portion wasn't programmed. 

    To be honest I can appreciate only the ECC part of the filled portion because of filled with 0xFF that's the erase value.

    Thank you again for your support

    Best Regards

    Silvano Battisti

  • Hello,

    We need help from CCS team. I don't know why the vfilled portion is not programmed sometimes.